Part Number: SN74CB3T3257 Other Parts Discussed in Thread: TS3A24157 , SN74AVC1T45 Hi,
We are using SN74CB3T3257PWR device. This is powered by 3.3V but the IOs we are providing is at 1.8V logic. Please share confirmation that this device supports 1.8V IO…
Other Parts Discussed in Thread: TS3A24157 Hello! In this occasion, i would like to implement a system which can let me switch automatically parallel to series mode of two batteries represented on the image as b1and b2.
The idea is to control it using…
Other Parts Discussed in Thread: DRV8839 , LM317M , TS5A23159 , TS3A24157 , TS3A27518E , MSP430G2553 Hi,
Iam looking for CAD/bxl files for
drv8839
ldc1000
lm317m
ts5a23159
ts3a24157
ts3a27518e
msp430g2553
Can someone please help me with a link to these…
Other Parts Discussed in Thread: TS5A23157 , ADS1298R , TS3A24157 , TS3A24159 Hello, I would like to switch/mux ADS1298R input channels to different signal sources, e.g. to switch between V6 electrode and respiration circuitry to channel 1. Switch should be…
Justin,
My recommendation would be to pick from TI's signal switch and multiplexer products .
It looks for your application you will need a 2 channel 1:2 mux or 2 channel SPDT configuration to switch the CAN high and CAN low lines from to two different…
Other Parts Discussed in Thread: SN65HVD232 , TS3A24157 I want to connect a microcontroller with two CAN channels to three different CAN networks, selected via code. Effectively, I want to multiplex my CAN transceivers.
For CAN1, I use the TI SN65HVD232…
Other Parts Discussed in Thread: TS3A24159 , TS3A24157 Hello My name is Hidetoshi Matusnami.
I would like to ask you the value of "Peak on resistance" and "Turn-on time” for TS3A24159 Date Sheet .
The value of "Peak on resistance" and…
Other Parts Discussed in Thread: ADS1298R , TS5A12301E Hello, I would like to switch/mux ADS1298R input channels to different signal sources, e.g. to switch between V6 electrode and respiration circuitry to channel 1. Switch should be dual SPDT digitally…
Hi Anton,
In general, the absolute maximum voltages for the outputs will be specified in the datasheet. For example, the dual SPDT TS3A24157 specifies the maximums on the NC and NO outputs on page 2 of the datasheet:
Voltages higher than specified here…