Hi Nir,
Thank you for your reply.
I understand there is no guarantee the outside of the recommended voltage range.
I'll share the information with the customer.
I appreciate your great help and cooperation.
Best regards,
Shinichi
Part Number: TS3A27518E Hi
I want to use Part No:TS3A27518ERTWR for our new design. but we don't find junction temperature in data sheet.
can you please suggest maximum allowable junction Temperature of TS 3A27518ERTWR
so that, that IC don't damage…
Part Number: TS3A27518E Other Parts Discussed in Thread: TMUX1574 , Tool/software: Hello,
I am attempting update a existing test system to be able to run 2 variants of boards. Each variant has its own firmware that needs to be applied via a SD card. Currently…
Part Number: TS3A27518ETS3A27518E S-Parameter model TS3A27518E_sParameters_25C.S2P does not simulate as the datasheet suggests it should. There is significant signal degradation at 100MHz. The datasheet says it has typical 4 ohm on resistance, and a bandwidth…
Part Number: TS3A27518E Dear Ti experts,
I have done a SPI memory circuits design using TS3A27518E. Attached the schematics design pdf file and high-level block diagram of the requirement. My intention is to flash the SPI flash memory via following method…
Part Number: TS3A27518E Hi, How to check IC date codes on such IC's There's inscriptions of YL518E 27K G4 (G4 is in smaller font and is underlined) AN5H
Part Number: TS3A27518E Other Parts Discussed in Thread: SN74AUP1G17 , SN74LVC1G17 As per the attached block diagram, I will connect A side at 1.8V (VCCA) domine and B side at 3.3V (VCCB). Can I give the 1.8V or 3.3V data randomly at VCCB side without changing…
Part Number: TS3A27518E Hi TI Teams,
Our project requires the use of two SPI flashes, compatible with wire brushes, and we plan to use two TS3A27518E for this application, the schematic block diagram is as follows:
Is this design feasible? Or do you have…
Hello Nirojan,
Nirojan Navaratnarajah said: From our side we tried to initialize the I2C driver and also created an instance of the IO expander using the driver from TI
Just to confirm here, were you using the drivers mentioned on this page: https://software…