Part Number: TS3DV621 Hi
Can we use AUX + / - pin as data input ? Also can we use D1 +/- pin as a clock input? (clock speed is 1GHz)
(The customer would like to swap between clock input of AUX pin and data input of D1 pin.)
Because as the PCB…
Part Number: TS3DV621 Hi
Regarding unused pin, can we leave those pins open if it is not used HPD pin and CEC pin?
Also, about band width of AUX+/- pin, how much band width can be allowed? Is it possible to use as a input of LVDS clock of 150MHz.…
Part Number: TS3DV621 Hi team,
I want to check whether the TS3DV621 can be configure like below?
1. Can D0 change the positon with D1?
2. Can D0+ change the position with D0-?
Thank you.
BR
Frank
Part Number: TS3DV621 Hi team,
We want to check whether the TS3DV621 can support 3840*2160 30frame rate HDMI or not. My customer want to use it as 4k HDMI switch, when test a port it doesn't pass. But B port pass the test. Does the A port have difference…
Part Number: TS3DV621
Hi,
I have to design one System which has requirements as given Below.
- Input: One HDMI Connector.
- Output: Three HDMI connectors.
-System Description :
Need to split this HDMI input to the three HDMI connectors.
…
Part Number: TS3DV621 Other Parts Discussed in Thread: TS3DV642 Hi team,
The TS3DV6421 12-channel Mux has ON-resistance listed on page 6 of the datasheet as follows: At Vcc=3V, the spec is 6.5Ω typical, 9.5Ω max over a Vi/o range of 1.5V to Vcc.
What…
Kensuke-san,
You are correct the TS3DV642 is the next generation device of TS3DV621. The TS3DV642 has many upgrades in performance to accommodate the newer HDMI 2.0 and DisplayPort 1.2a requirements. The reason for the pinout change is to improve the…
Hello Dan,
You bring forth an issue that is persistant for the TS3DV621.
Unfortuntaly, there is no recommended way to wire this part in a way that makes the trace patterns less awkward (In my opinion you did a smash up job considering how this pinout…
Part Number: TS3DV621 Other Parts Discussed in Thread: SN65LVCP114 Hi team,
My customer want to use the the device TS3DV621RUAR to do MUX function for GPHY. Can the device support the function or do we have other solutions?( For the red circuit part…
Hello Andrew.
What is the maximum bandwidth of AUX+/- channel of TS3DV621? We would like to use it for MIPI DSI interface that utilises 4 data lanes and one clock lane. All of them require 1GHz.
Roman.