Part Number: TS3DV642-Q1 Other Parts Discussed in Thread: TS3DV642 Hello,
I have a aplication with LVPECL signals where i am considering useing TS3DV642-Q1.
Can TI please confirm if this chip is suitable for this situation. My datarate is 1300Mbps…
Part Number: TS3DV642-Q1 It is used for MIPI signal switches.
Is it okay to connect a negative signal to the + pin and a positive signal to the - pin?
Please provide an answer. Thanks!
Part Number: TS3DV642-Q1 Tool/software: HI team, Can you please provide SNP model for the above mentioned MIPI switch TS3DV642-Q1. As the available model on website contains only LTspice netlist, Alitum library file, along with a pdf file. Please do the…
Hi Kevin,
The TS3DV642-Q1 supports differential bandwidths of -3dB from DC up to 5.8GHz so there should not be any bandwidth issues.
Since you are using it for a DSI based application, I would recommend connecting the DSI CLK+ signal to the switch…
Part Number: TS3DV642-Q1 Hello,
I am using 12-channel MUX (TS3DV642RUATQ1 ) to multiplexing between eMMC device and microSD card. for this application, I have to connect CLK, CMD and DM (data Mask) pins to SCL, SDA, HPD and CEC pins of this MUX. The…
Part Number: TS3DV642 Tool/software: Hi, can you please confirm that TS3DV642A0RUAR and TS3DV642RUARQ1 have the same Silicon and package?
The industrial version is out of stock and for my prototypes I need to use the Q1, but need to make sure there…
Part Number: TS3DV642-Q1 Hello team,
Do you have S parameter model? My customer want to do SI simulation for SoC-TS3DV642 DP line.
Regards,
Youhei MIYAOKA