Part Number: TS3USB221A Hi,
I have a little complex USB port design and I was wondering if my design is ok.
I have two USB connectors 1 and 2. MCU input also has 2 USB inputs but one High Speed and one Full Speed.
I will be using FS USB only on certain…
Part Number: TS3USB221A-Q1 Hi all,
My customer is using TS3USB221A-Q1 for their ESD protection. As I know, spec shows "ESD Performance I/O to GND Per JESD 22 – 12-kV Human-Body Mode" Contact discharge could meet the requirement, but I…
Part Number: TS3USB221A Other Parts Discussed in Thread: TS3USB30 , TS3USB221E Hi team,
Can TS3USB221A connect to two hosts?
As I saw in TS3USB30 datasheet, it clearly written that The device multiplexes differential outputs from a USB host device to one…
Part Number: TS3USB221A Are we allowed to swap D+ and D- on the TS3USB221ARSER if we swap them on all the INs and OUTs? So basically all the D+ pins on the part get connected to D- signals on the PCB and all the D- pins get connected to the D+ signals…
Part Number: TS3USB221A-Q1 Hi team,
I'd like to double check if the 1.8V level from CPU can be used at S pin control of TS3USB221A-Q1, when using Vcc=3.3V and OE pin connected to GND.
Can you please answer it?
Thanks,
Sam Lee
Part Number: TS3USB221A Other Parts Discussed in Thread: TS3USB221 Hi:
We are using the IC TS3USB221ARSER, and I have a question about it.
We know this IC is a USB switch, could we exchange the D+ and D- of the Common Port and Port ,1 Port2, just like USB_DPs…
Part Number: TS3USB221A Other Parts Discussed in Thread: TS3USB3000 , TS3USB221 Hi,
I would like to get a clarification on the I/O of the TS3USB221A if it's compatible with 5V level input/output voltage.
With reference to the datasheet, we got to…
Part Number: TS3USB221A Other Parts Discussed in Thread: TS3USB221 Hello
If all Common USB Port and USB Port 1,USB Port 2 's D+ and D- was all inverse connection , is it ok for this connection ?
Hello Matt,
The design of using the VCC3V3 for TVSP8 on this EVM is specifically intended for the TPS25772Q1EVM-CD-150.
The TPS25762Q1EVM, TPS25772Q1EVM-CO-149, and TPS25772Q1EVM-CD-150 are 3 variants of the same EVM design. The BOM are different to evaluate…