Part Number: TS3USB221A-Q1 Hi
In the figure below, USB Slave on the left, USB Host on the right,
It's a high-speed analog switch that does a two-channel switch,
The host and slave should be unrelated. Is this a correct connection?
thanks!
Part Number: TMUX4052-Q1 Other Parts Discussed in Thread: TMUX1309-Q1 , TS5A23157-Q1 , SN74LVC2G17 , SN74LVC1G08 , TS3USB221A-Q1 Find a URAT MUX,One Chanel URAT is converted to two outputs, 2chanel,2:1MUX,automotive application
Part Number: TS3USB221A-Q1 Hi sir,
In the table there are the same value 2000V for HBM and for CDM. Is it possible?
We checked this classification C5 and found the ESD values(750 V to < 1000 volts) in the AEC-Q100 documentation.
Please confirm.
Thank…
Hi Gareth,
Please look at the TS3USB221A-Q1. This has a TA of up to 125 degrees Celsius: https://www.ti.com/product/TS3USB221A-Q1
Please let me know if that works for you, and if not, I can keep looking.
Thanks,
Ryan
Part Number: TS3USB221A-Q1 we’d like to find these two parts with wettable flank package. Could you please help to check it? If not, please help to suggest alternative solution for us.
Update one thing the package with lead pins is also acceptable…
Part Number: TS3USB221A-Q1 Other Parts Discussed in Thread: TS3USB221 Hello Experts, Do you have an IBIS model for TS3USB221AQRSERQ1? I don't found it up in TI.com. I may use TS3USB221 IBIS model for signal integrity check of TS3USB221AQRSERQ1? Best Regards…
Part Number: TS3USB221A-Q1 Hi all,
My customer is using TS3USB221A-Q1 for their ESD protection. As I know, spec shows "ESD Performance I/O to GND Per JESD 22 – 12-kV Human-Body Mode" Contact discharge could meet the requirement, but I…
Part Number: TS3USB221A-Q1 Hi team,
I'd like to double check if the 1.8V level from CPU can be used at S pin control of TS3USB221A-Q1, when using Vcc=3.3V and OE pin connected to GND.
Can you please answer it?
Thanks,
Sam Lee