Part Number: TS3USB221 Hi
The TS3USB221RSER schematic is shown in the diagram below. It is used to switch between USB 2.0 D+/D- and UART debug TX/RX outputs to the USB Type-A connector.
The UART (UART1_TX_3V/UART1_RX_3V) is connected to the CPU i…
Part Number: TS3USB221E Other Parts Discussed in Thread: TS3USB221 , , TS3USB221A Tool/software: Do you have availability difference between TS3USB221 and TS3USB221E?
Part Number: TS3USB221 TS3USB221RSER We observed that the Xray resuts different from our previous records. 2602+ XRAY diferent with 2607+,Is it caused by changes to the PCN? thanks!
Part Number: TS3USB221 Hi team,
My customer has been looking for 4:1 USB2.0 MUX/DEMUX and uses 3pcs of TS3USB221 to achieve it like the figure below. Is this circuit configuration acceptable?
2. TS3USBCA420 is 4:1 MUX. Is it possible to use…
Part Number: TS3USB221 Hi
My customer is affected by the PCN : 20240724002.1 and PCN : 20241101001.0
Their product is failing some production test post PCN
They woudl like to compare past Datasheet versions for the parameter, to check on their…
Part Number: TS3USB221 Tool/software: Hello experts,
I had a quick question about Ron of TS3USB221,
On datasheet it mentions Ron (typ, max) when Vcc=3V, 2.3V (Vi=2.4V, Io=-15mA) .
Customer asked, if it would have the same Ron (typ, max) when Vcc…
Part Number: TS3USB221 Tool/software: Dear support center department.
I hope all is well with you.
Regarding PCN# 20240724002.1 ,
could you submit the "PCN Supporting Data Package".
In particular, document relating to:
1. X-ray
2. Wirebond…
Part Number: TS3USB221
Hi Team,
Customer would like to design 1:2 MUX TS3USB221.
Would you please help review and let us know any difference?
Thanks for help!
SHH