Part Number: TS3USB30E S parameter file: D1_4V3-D1-thru-D.S4P
how to correspond the port(0,1,2,3) of S parameter file to D1+,D1-,D+,D-?
2. Can the frequency response of S parameter mode extend to 20GHz??
Part Number: TS3USB30 Other Parts Discussed in Thread: TS3USB221 I was about to route differential pairs for the 2:1 USB mux "TS3USB30" but then realised it's impossible. The pins for "device 1" and "device 2" are not in pairs, so how am I supposed to…
Part Number: TS3USB30E Hello,
I have discovered that there are some things that are not correct in the latest version of the TS3USB30E datasheet, version G, and I hope you can provide some clarity on what is correct.
It says in the text in several…
Part Number: TS3USB30 Tool/software: Hi Team,
TS3USB30E -3DB bandwidth According to the measurement method provided on specifications, it is to continuously increase the signal frequency at the input end until 900Mhz to observe whether the output amplitude…
Part Number: TS3USB30E Other Parts Discussed in Thread: TMUXHS221 Dear Team,
May I ask how much Jitter and Latency will be added if it is used as a PCIe Gen5 CLK to channel switch?
Many Thanks,
Jimmy
Part Number: TS3USB30E Other Parts Discussed in Thread: SN74LVC2G66 Tool/software: Hello support team,
I'm looking at using the TS3USB30EDGSR to disable a UART connection to host while the host is being programmed, or if the UART device is powered off…
Part Number: TS3USB30 Hello Team,
some muxes support break before make and a little output voltage drop is observed at switching time.
Can you confirm that TS3USB30 does not support break before make, please?
Thank you and Best Regards, Hans
Part Number: TS3USB30 Dear Specialists,
My customer is looking for SPDT switch.
Could you please advise recommended device.
--
I'm looking for Switch between two hosts (PCs) and use one printer. Please introduce the USB 2.0 (480Mbps) 1:2 multiplexer…
Part Number: TS3USB30E Other Parts Discussed in Thread: TS3USB221A , , TS3USB221 I see for operating voltage, it’s recommended for Data input/output to stay within VCC. My customer has some corner cases where Data may be 70mV above VCC, but is current…