Part Number: TS3USB3031 Other Parts Discussed in Thread: TS3USBA225 Hi team,
For either TS3USB3031 or TS3USBA225, when VCC is low, is there any back current concern between Diff pair I/O and VCC? Also between Select I/O and VCC?
Thank you!
Austin…
Part Number: TS3USB3031 Other Parts Discussed in Thread: TS3USBA225 , Hi all,
If the chip is powered by 3V, while the USB2 I/O inputs see 3.3V, will this work okay?
Thank you,
Austin Allen
Part Number: TS3USB3031 Hi team
In customer's application, 2:1 USB switch is phase out, they need at least 1:3 USB switch.
I find the only device that might fulfill the requirement is TS3USB3031, but one channel is for HML.
Can TS3USB3031 support…
Part Number: TS3USB3031 Other Parts Discussed in Thread: TMUXHS4212 ,
HI,
My name is Kang eungu
I will use TMUXHS4212, TS3USB3031
TMUXHS4212 and TS3USB3031 have ESD Protection Diode
if it have, I ask Specification such as Positive Diode…
Part Number: TS3USB3031 Hi Expert,
I didn't see Tj information in datasheet, could you help to share it with me?
what's the maximum power dissipation for this device? how to calculate?
Regards,
Mark
Part Number: TS3USB3031 Dears
For the TS3USB3031 chip, must the pin d+, d- correspond to the USB d+, d-? If it is reversed, what effect will it have on the USB data transfer (as shown in the figure below)? If data communication is not carried out, only…
Part Number: TS3USB3031 Hi Experts,
Our customer wants to use the TS3USB3031 in I2C switch application as below, from the datasheet description, it looks like we can support it. Now the question is, may I know when USB1+/1- channel is selected, what…
Part Number: TS3USB3031 Hi,
I know that the HSpice Model is available in TI.com but can you provide S-parameter for TS3USB3031?
Best Regards,
Satoshi / Japan Disty
Part Number: TS3USB3031 Hi team,
1. Regarding the switch, TS3USB3031RMGR, dual-channel 1:3, if use it for switching 3 different LVDS signals, the maximum speed of them is 2.5Gbps, can this chip support that founction? if not, could you recommend some…
Part Number: TS3USB3031 Other Parts Discussed in Thread: HD3SS3212 Hi
The spec this part shows the USB lines have the bandwidth of 6.5Ghz. With this kind of bandwidth, can we use this particular part for USB3.1 Gen1(5Gps or 2.5Ghz) application? If this…