Part Number: TS3USB3200 Other Parts Discussed in Thread: TMUX136 , TS3DDR4000 , HD3SS3412 , TS3DV642 , DS42MB200
H Team,
Our customer is looking for a VBO-HS splitter to distribute the signal into 2 outputs. According to our customer,
VBO-HS maximum frequency…
Part Number: TS3USB3200 Team,
What is the difference between TS3USB32008RSVR and TS3USB3200RSVR. Can't find it in the documentation we have.
The only difference I found is top side marking, and I am not sure what it signifies.
Thanks
Viktorija
Part Number: TS3USB3200 Other Parts Discussed in Thread: TS5USBA224
Hi Team,
customer is looking for 2:1 mux for I2S data pin application. Can TS3USB3200 support I2S Data pin swtich?
BR, SHH
Part Number: TS3USB3200 I am currently using the TS3USB3200 on my prototype board. I needed a 2:1 USB switch with ID line. I have read the finer details of the datasheet and come to find out that one port is meant for MHL signals. My application requires…
Part Number: TS3USB3200 Hi,
Can we use TS3USB3200 as a UART MUX instead of USB MUX? What should we take care specifically if it's used as a UART 1:2 MUX?
If not, what's better solution from TI for UART MUX?
Thanks!
Antony
Kai,
Yes we have several products that could support 2.25Gbps. For this data rate we recommend you select a switch with a bandwidth > than 3.4 GHz (you can see our multiplexer FAQ thread for more information on the data rate to bandwidth conversion…
Arthur,
The TS3USB3200 cannot be powered with 9V since the datasheet abs max is 5.5V. Here is a blog post about using the TS3USB3000 to protection processors from a 9V short in USB connector during fast charging mode.
Thank you,
Adam
Hideto,
[Q1] Is TS3USB3200 available with MHL SINK apparatus?
The TS3USB3200 devices is an unbuffered pass FET so it will not sink current through the singal path but rather pass it from the input to the output.
【Q2】 Does TS3USB3200 perform Pulse/Discovery…