Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: TS3USB3200 , SN74CBTLV3257 , TS3A5018
We are looking for more information regarding any mux switches for SPI that TI carries. These are the specs we are looking for:
3PDT (2 x DPDT could also work)
BW >= 100 MHz
Ron…
Part Number: BQ25606 Other Parts Discussed in Thread: TS3USB3000 , TS3USB3200 Hi,
I´m currently working on a schematic for an embedded device which should commuicate to the PC via USB and should be powered by a battery pack charged via the BQ25606. So…
Other Parts Discussed in Thread: TS3USB3200 I need:
1-differential pair (6Gbps) with min voltage of 1.635V and Max = 3.485V 1-single ended signal (75mbps) with min voltage of -0.03V and Max = 0.83V.
I took a look at TS3USB3200 and could not find eye diagrams…
Other Parts Discussed in Thread: TS3USB3200 Hi team,
My customer is planing to use TS3USB3200 as below application.
And they also need HDMI to MHL Bridge device, is there any device that can support HDMI to MHL Bridge function?
Thanks.
Prescott
Other Parts Discussed in Thread: TS3USB3200 I am trying to select an analog switch and high bandwidth (>>100MHz) is a critical parameter. But the parametric guides do not include bandwidth or capacitance as criteria. Any suggestions on how to proceed…
Other Parts Discussed in Thread: HD3SS6126 , TUSB8041 , TUSB8020B Dear Sir/Madam/Miss,
Do HD3SS6126 chip support for 8:1 multiplexer (USB 3.0)? Since its only designed for 2:1/1:2, I'm wondering can I cascade it into 8:1.
Is that will be a problem in…