Other Parts Discussed in Thread: TMUX2889 , TS5A23160 , TMUX1072 , DRV2605 , TS5A26542 , TMUX6234 part number: TMUX2889
Hi TI,
In the TMUX2889 datasheet page. 10 - Figure 6-14. Insertion loss versus frequency,
We can see there is no insertion loss…
Part Number: TS3A4741 Other Parts Discussed in Thread: TMUX1208 , TS3A27518 , TS5A26542 Hi Team,
I would like to know if TS3A4741 the supply current increases from less than 1µA to >50µA if VDD 3.3V is used together with 1.8V Logic similar to TMUX112x…
Hi Tushar,
Most signal switches are used in 50-500mA applications.
Have you looked at the TS5A26542 - it has very low RON of 0.5 Ohm (typ) and supports current upto 450mA.
For more than 500mA, you would need to look into power switches - in that…
Hi Aravind,
Thank you for your patience, the holiday weekend has slowed down getting back to you.
I went through and filtered our product selection table for SPDT devices that operate at both 3.3 and 5.5V. Looking at our results for these SPDT devices…
Fernando,
The TS3AXXXX devices will not be suitable for you application because these are 3V supply switches. The TSXXXXXX family of products has the first number as the voltage supply so you will need to find a TS5XXXXX device support your 5V supply…
Hi Ranita,
The ADG1633 is a 3-channel SPDT switch. We do not have many 3-channel devices currently in our portfolio. Of those we have the SN74LV4053A has an Ron around 20ohm with a sup[ply range of 2-5.5V. We also have the CD4053 that has a much higher…
Other Parts Discussed in Thread: HD3SS6126 , TUSB8041 , TUSB8020B Dear Sir/Madam/Miss,
Do HD3SS6126 chip support for 8:1 multiplexer (USB 3.0)? Since its only designed for 2:1/1:2, I'm wondering can I cascade it into 8:1.
Is that will be a problem…