Part Number: TS3A4751 Other Parts Discussed in Thread: TS3A44159 , AFE4410 , TS5A26542 , TS5A6542
Dear Sir,
I have to control the output voltage (which is very low) of 2 sensors and the input voltage of 2 pairs of red/ired leds. It is for a low-power wearable…
Other Parts Discussed in Thread: TS5A12301E , TS5A6542 , TS3DS10224 , TS3A5017 , TS5A9411 My customer is asking for technically comparable part to the MAX4564 and MAX4634 (perhaps with better specs - lower power/wider temp range)? It doesn't have to be pin…
Other Parts Discussed in Thread: TS5A6542 , TS5A12301E , TS5A9411 Hello,
I am looking for a 1 channel SPDT analog switch (3.3V, 50 Ohm max) with low leakage (1 uA max) and an enable. I have narrowed in on the list of parts below, but wanted to run this…
Other Parts Discussed in Thread: TS3A44159 , TS5A6542 , TS3A24159
I am looking for a 2input /1output Mux switch for 1pps signal. LVCMOS signal and 3.3 operating voltage.
Is there anything in your product line that can meet these specs?
Other Parts Discussed in Thread: TS5A6542 , TS5A12301E , TS5A3167 , TS5A3166 , TS5A9411 Hello,
I need to see if the TS5A6542 can accept 3.0 volts on the V IO pin. I need to switch 4.0 volts with a control voltage of 0 or 3.0 volts and must avoid the increased…
Hello Alvaro,
Would it be possible for me to get a schematic of your circuit so I can clearly understand your setup?
If I am understanding you correctly, when you take away the transient protection (diode array) from the circuit, the circuit can pass your…
Rian,
The TS5A6542 accepts control line voltages from 1.65V to 1.95V. Please look at the following link for the datasheet.
http://www.ti.com/product/ts5a6542#technicaldocuments
Regards, Alex
Other Parts Discussed in Thread: HD3SS6126 , TUSB8041 , TUSB8020B Dear Sir/Madam/Miss,
Do HD3SS6126 chip support for 8:1 multiplexer (USB 3.0)? Since its only designed for 2:1/1:2, I'm wondering can I cascade it into 8:1.
Is that will be a problem in…