Part Number: TSB41BA3B-EP I need an IBIS-AMI model for simulating a PCB signal integrality.
Device name of the model I am requesting:TSB41BA3B-EP
Best Regards,
Mandy
Part Number: TSB41BA3B-EP Other Parts Discussed in Thread: TSB41BA3F-EP Hi team,
What is the junction to board (Theta_JB) and/or the junction to case bottom (Theta_casebot) thermal resistance for this component (TSB41BA3BTPFPEP)?
Also, what is the maximum…
Part Number: TSB41BA3B-EP Does the TSB41BA3BTPFPEP support the hot swap function?
Can a 1394 input be applied with power removed on this device? If so, where is this stated in the datasheet (the ABS max table indicates inputs < Vdd + 0.5V)?
Part Number: TSB41BA3B-EP Hi all:
I use TSB41BA3B-EP to design a 1394 distributor, that is, the 1394 signal source sends data to port0, and port1 and port2 are connected to two devices to receive the data from the signal source. During the test, it was…
Part Number: TSB41BA3B-EP Team,
What is the EXACT recommendation for creating the footprint specifically the center plane copper and solder mask dimensions?
What is the EXACT paste aperture recommendations for 4 mil, 5 mil and 6 mil foils for the center…
Part Number: TSB41BA3B-EP Team,
If we have the BMODE pin pulled low (deasserted), can we still have differential input voltages of 800mV?
From page 16 of the datasheet:
Also, what is the maximum differential voltage that is allowed on the PHY before…
Part Number: TSB41BA3B-EP What is the typical current for DVDD-CORE (we are considering using an external DC/DC to save power vs using the internal regulator)?
Part Number: TSB41BA3B-EP Hi team,
Do either the Link Layer or PHY chips have any type of internal Loopback Mode?
I know there is a TestMode input and its not recommended for user use, but does that have the Loopback Capability?
Thank you.