Part Number: AM3352 Other Parts Discussed in Thread: WL1831MOD , I have a custom board that has an AM3352 and WL1831MOD on it, wired up exactly like the EVK and MOD8 board. It does seem to be mostly working but the data wlan interface seems very unstable…
Part Number: AM4378 Tool/software: We are working on am437x based custom board, Migrating from 4.19 to 6.1 kernel. I updated the dts changes specific to ethernet & cpsw switch taking am437x-sk dts as reference.
After updating my dts ethernet phy's are…
Hi Praveen,
As shown below:
I have check all CONFIG_USB_* entries in kernel3.14 configuration, They are the same。
kernel3.14 configuration:
#
# Automatically generated file; DO NOT EDIT.
# Linux/arm 3.14.63 Kernel Configuration
#
CONFIG_ARM…
Part Number: AM625 Other Parts Discussed in Thread: DP83620 Hi,
i am using am625 hs-fs custom board based on processor sdk 8.06.00.042. could you any one suggest how to resolve the following kernel crash issue,
[ 11.264823] davinci_mdio 8000f00.mdio…
Part Number: PROCESSOR-SDK-AM64X I am working on porting device trees from a device that was originally brought up on the 08.00.00.21 SDK So far I am able to boot and use the Ethernet device, but I do not see any PCI devices in `lspci` or in /sys
Diff…
Part Number: PROCESSOR-SDK-AM335X Other Parts Discussed in Thread: AM3352 Tool/software: Hi, all.
I caught the problem with the watchdog using on AM335X cpu.
We use the kirstone yocto build. Version of kernel is 6.1.33.
Log and kernel crash is below…
Part Number: J784S4XEVM Related to this older thread, I'm also trying to get uvc-gadget to work, on a J784S4XEVM this time. My script is listed below.
#! /bin/sh
GADGET_DIR="/sys/kernel/config/usb_gadget"
GADGET_NAME="uvc_gadget"
LANGUAGE=0x409…
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62 , SK-LCD1 , SK-AM62B-P1 Tool/software: I am trying to use dual OLDI displays on the AM6254ATCGGAALW.
I do not see tidss initializing upon boot as is stated in SDK documentation section 3.2…
Part Number: PROCESSOR-SDK-AM335X Other Parts Discussed in Thread: AM3352 Tool/software: A custom board reference to am335x-evm,
With cryptodev enabled and watchdog disabled in Linux kernel 6.1.33 , the kernel boots up properly with a cryptodev module…