Part Number: TSER953 Hi,
We are using the V3-Link serializer (PN: TSER953) for our cameras. The cameras will be used in a high vibration automotive environment. Initially we found a capacitor short (C15 capacitor) issue in few cameras. The schematics…
Part Number: TSER953 Other Parts Discussed in Thread: DS90UB953-Q1 Tool/software: We are using TSER953 serializer is our custom board for automotive application. But as per the datasheet of TSER953 serializer, the temperature range is -20 to +85degreeC…
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 , DS90UB954-Q1 , DS90UB953-Q1 Hi All,
I have some questions regarding the TSER953 and TDES954.
I understand there are no planned end-of-life (EOL) dates for the TSER953 and TDES954, but…
Part Number: TSER953 Hi There, we have designed a FPD-III Link Serializer (TSER953) camera with compatible Deserializer. The strap pins are mounted for Synchronous mode in both Serializer and Deserializer. We have also provided an external clock of 25MHz…
Part Number: TSER953 Other Parts Discussed in Thread: DS90UB960-Q1 , DS90UB953-Q1 , DS90UB960-Q1EVM Hi There,
We are using the DS90UB953-Q1 Serializer on our camera board and the DS90UB960-Q1 Deserializer on the carrier board. The FPD-Link III connection…
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 Tool/software: I am currently working on a setup involving the V3 Link Adapter Board connected to a Raspberry Pi 4. The TSER953 serializer and the TDES954 deserializer are connected via a coaxial…
Part Number: TDES954 Other Parts Discussed in Thread: TSER953 We have ser input -> deser output working and now would like to get deser input -> ser output gpio working thanks.
#!/usr/bin/env python3
import smbus2
import time
from smbus2 import SMBus…
Part Number: TSER953 Hi Team,
I am using below mentioned poc circuit. I have some questions regarding that poc circuit.
My requirement for PoC circuit is:
Current= 500mA
Temperature rating= -20'C to 55'C
Frequency: 25MHz to 2.1GHz
Query…
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 Tool/software: Is there a good way to isolate the V3Link signal between the TSER953 serializer and TDES954 deserializer? Normally, I would use a high speed LVDS isolator, but the V3Link signal…