Part Number: TSER953 Other Parts Discussed in Thread: TDES954 Hello:
For TSER953 and TSER954, Can these two chips support a 50M MIPI camera? such as OV50H
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: TSER953 , TDES960 ,
Tool/software:
I flashed the linux image ( tisdk-edgeai-image-am62axx-evm.wic.xz ) for am62a board with v3 link d-ch adapter board connected with 4 imx219 cameras , and…
Part Number: TSER953 Hello,
I am interested in mounting a bare die TESR953 Unfortunately, there is no pad information given in the datasheet. Could you tell me:
- bondpad metallization material
- thickness of bondbpad
- size and position of the…
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 Hi,
We have used TSER953 and TDES954 for 1920x1080p60 RAW10 video in the past successfully.
Now we are doing 3840x2160p30 RA10 and having an issue. Frame sync broken and sometimes partial…
Part Number: TSER953 Tool/software: I am getting the error "reason": "Product requested quantity is less than or equal to zero", "message": "Resubmit the request. Enter a quantity greater than zero", "data" even though i am entering quantity as 30000…
Part Number: TSER953 Hi Team,
I am using TSER953 part for CSI2 single lane mode.
Can you please tell me the current consumption for using only single lane.
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 Hi,
Please advise the below support need:
1. We use the TSER953 & TDES954 for camera signal Serializer and Deserializer, we wants to know there are any test equipment promote to measure…
Part Number: TSER953 Hi,
I'm thinking of using the TSER953 to transmit MIPI CSI-2 over long distances. Is it possible for the TSER953 to convert low-rate signals such as MIPI CSI-2 640 x 480 30fps to V3Link and transmit them?
Similar products from…
Part Number: TSER953 Other Parts Discussed in Thread: TDES954 I have CSI-2 with 600Mbps/lane and 4 lanes on TSER953 input port. I configured the TSER953 trough des TDES954. TSER953 is on RX0. i2c addr tdes: 0x68, i2c-addr tser: 0x30. i2c transfers:
…