Part Number: TSM24CA-Q1 Tool/software: Hello everyone,
i just downloaded the SPICE model of the TSM24CA-Q1 as well as the corresponding data sheet. However, it seems that there are some inconsistencies between the datasheet and basic diode model that…
Part Number: TSM24CA-Q1
Tool/software:
Dear team,
Do TSM24CA-Q1 or any other TVS from TI support IEC60060 impulse test? Detail is not disclosed but pulse width = 1us, pulse frequency = 10ms, peak voltage=+/- 2kV is applied via coupling capacitor…
Part Number: TSM24CA-Q1 In the datasheet it has been mentioned as,
Maximum Reverse stand-off voltage (VRWM) as +24V.
Minimum Breakdown voltage (I/O to GND and GND to I/O) as +25.5V ( with the test condition of only 10mA of current ).
We are…
Part Number: TSM24CA-Q1 Other Parts Discussed in Thread: TSM24CA , TPD1E01B04-Q1 , TPD4E02B04-Q1 Tool/software: I am searching for an alternative component of the ESD diode. But I found that although the clamping voltage is the same, the test current…
Part Number: ESD2CAN24-Q1 Other Parts Discussed in Thread: ESD2CANFD24-Q1 , ESD2CAN36-Q1 , TSM24CA-Q1 Tool/software: Hello team,
There is a failure under BCI 300mA for ESD2CANFD24-Q1, customer found ESD2CAN24-Q1 can understand higher current and power…
Part Number: TCAN1044V Other Parts Discussed in Thread: TSM24CA-Q1 , TSD12C-Q1 Tool/software: Hi team
I am using the TCAN1044 in our design.
For the Protection diodes what are the parameters need to include in the selection.
In the reference design…
Part Number: TPD1E10B09-Q1 Other Parts Discussed in Thread: TSM24CA-Q1 , TSM24CA Hi team,
My customer AUO is working for the Geely automotive display platform and we use TPD1E10B09-Q1 in their previous design for 6.3V power rail.
Now they change…
Other Parts Discussed in Thread: TPD1E10B06-Q1 , TSM24CA-Q1 , ESD2CAN24-Q1 Hi Team,
Could you pls help recommend an auto alternative for MLSEP05A-0402, SMBJ30CA, WPE24CT23BL-G? Thanks!
Regards
Hailiang
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…