Part Number: TUSB1002 Hi Expert,
Since the layout guideline only said that it recommended to keep the via count to 2 or less.
May I know what happens if I need more than 2 vias?
From my perspective, more vias means more insertion loss, so if i need more…
Part Number: TUSB1002 Hi,
Due to the board is large and there is 2 cascaded hub in system, my customer put a TUSB1002 close to up port hub.
Can I know if there is any way to check the TUSB1002 eq\gain setting is good enough?
Do we have data for the eq…
Part Number: TUSB1002
Hi -
We are trying to layout the traces for the TUSB1002 chip and I am looking at the design recommendations in the TI docs. Which states: Each pair should be separated at least by 3 times the signal trace width. However the recommended…
Part Number: TUSB1002 Until now we have been using your USB 3.0 hubs to amplify the signal. Currently there is a re-design and we would like to get away from the hub and use your Redriver TUSB1002.
For first tests we have ordered 2x TUSB1002EVM. We have…
Part Number: TUSB1002 Other Parts Discussed in Thread: TUSB522P , , Dear team
Does TUSB1002RGET and TUSB522PIRGER could replace each other?
Many thanks
Denny
Part Number: TUSB1002 Hi Ti team,
In our previous project we used TUSB1002R for re-driver purpose with USB3.1.
Now we want to support USB4.0 with 40Gbps speed. Can you suggest part which is suitable for our application and also support 40Gbps speed.
Part Number: TUSB1002 If I'm only interfacing with a SATA device, and I limit the AC coupling caps on the device side to less than 12nf, are the ferrites and fets needed as shown on the data sheet figure 22?
Part Number: TUSB1002 Please explain the behavior of the CONGIG PINS internal PULL-ups/downs and the timing of the sampling of these pins.
The statement below from the datasheet seems to imply that the internal PULLS on the config pins would be ACTIVE…
Part Number: TUSB1002 Other Parts Discussed in Thread: , TUSB522P ,
Hi, I am going to use TUSB1002 for my usb 3.2 device.
I have 4 questions for using this. Please help me.
-----------------------------------------------------------
Tusb1002 has too…