Part Number: TUSB1002A Tool/software: Hello,
I am designing a long meter cable that consists of 3 different junctions. See the image below for reference:
I know when creating a USB A to USB B cable the RX and TX switch, which happens on the redriver…
Part Number: TUSB1002A Other Parts Discussed in Thread: TUSB522P Tool/software: Hi TI Expert
Our placement is below, total trace length from Jeston Orin (host) to type-c connector is around 12.3 inch, which is over Jeston Orin's layout guidance (maximum…
Part Number: TUSB1002A Tool/software: Hi Team,
The datasheet of the TUSB1002A shown that the minimum length of Lac-cap to be 0.25 inches. If the layout space is limited and the distance between CAP and re-driver is less than 0.25 inches (not meeting…
Part Number: TUSB1002A Tool/software: Hi Team,
Datasheet shown that pin19/20 as TX and pin22/23 as RX, if customer want to use the function, does the PIN12/11 and PIN8/9 need swap it?
Many thanks~
Part Number: TUSB1002A Designing an USB 3.2 isolator and would like to know how to use two TUSB1002A on each side of the isolation barrier?
How does the automatic RX termination and RX detection work when two TUSB1002A are tied in series?
I am having…
Part Number: TUSB1002A Tool/software: Hi team.
I think customer can choose EQ8 for CH1 and EQ4 for CH2, correct?
Which CFG should they select? I don't konw how to select it.
Part Number: TUSB1002A Tool/software: Hi,
I would like to confirm what AC cap should be used for TX to host.
As the USB3.2 standard and CPU (host) vendor recommend to use 330nF. But in TUSB1002A suggest to use 220nF.
Please clarify.
Thanks.
Part Number: TUSB1002A Tool/software: Hi Team,
Pre channel loss 11.47dB ,Po st channel 2.23dB; customer want to check if TUSB1002A can support it. would you please help me check it?
Customer want to check the EQ setting, do you have any suggestion…