Part Number: TUSB1002A Does TUSB1002A recommends using of common mode choke for TX & RX?
We are planning to use TUSB1002A between host and the connector.
Regards,
Chandra
Hi,
Please see attached USB.org ECN on the optional 330nF for the SuperSpeed RX pins.
5684.USB 3.1 ECN Rx AC Coupling Capacitor Option.pdf
There are three implementation options for USB connector to the SuperSpeed RX pins:
1. DC couple the RX…
Part Number: TUSB1002A Other Parts Discussed in Thread: TUSB1002 , Hello,
I'd like to know about the differences between TUSB1002 and TUSB1002 A . I cannot exactly figure it out from the data sheets. It'd be helpful if a comparison table is available…
Part Number: TUSB1002A Hi Sir,
One of our customer's notebook project, due to the design of the SS USB cable is too long, and through the FPC to connect a small board. Now encounter some problem as follows:
When downloading with the USB3.0 port…
Part Number: TUSB1002A Hi Experts,
TUSB1002A document mentions an optional pulldown resistor, 220kohm, for RX port for discharging . I would use TUSB1002A with HD3SS3320, Type-C MUX, for Type-C configuration. In this case, should I consider about this…
Part Number: TUSB1002A Other Parts Discussed in Thread: TUSB522P , Hi TI team,
I plan to change TUSB522P to TUSB1002A.
I know that these two devices can accommodate similar designs.
In that case, Is it okay if the positional relationship between…
Part Number: TUSB1002A Hi TI Teams,
Can u help to check the schematic of TUSB1002A? The schematic is as below:
In addition, when debugging USB3.1 eye map signal, how to configure EQ1-EQ2 and CFG1-CFG2 of CH1&CH2 to improve the quality of eye…
Part Number: TUSB1002A Dear team,
My customer want to use TUSB1002A for 10G-KR(ethernet) interface. Is this possible to use TUSB1002A in other interface application?
Per my understood, we need to check data rate/ Swing/ common voltage which can…