Part Number: TUSB1044 Other Parts Discussed in Thread: TUSB1104 Hi,
In our design, the TUSB1044 is configured with a PD controller. If we do not want to use the PD controller functionality and intend to use the device only as a redriver for USB Type…
Part Number: TUSB1044 Other Parts Discussed in Thread: , TUSB1146 , TUSB1064
Hi Team,
We are currently developing a laptop using an Intel chipset with two Type-C ports:
TCP0 (Port 0) – Connected with a TUSB1044 redriver
TCP1 (Port 1)…
Part Number: TUSB1044 We tried to configure the TUSB1044 redriver from the CYPD6228-96BZXI using the I2C Communication.Even after sending the data to the appropriate registers which includes the:
REGISTER Data
General_3 Register(Offset = Ch) 0x68…
Part Number: TUSB1044 Tool/software: HI TI team We are working on the laptop project in which we need two type c connector with full functionality (Power + DP ALT mode), we have made the schematic based on CYPD6228, kindly help to review the schematic…
Part Number: TUSB1044
Tool/software:
HI
We have designed the schematic with TUSB1044, We are working on the laptop project in which we are planning to use the two type C with full functionality (I.e USB + Alt mode + PD functionality)
Please check…
Part Number: TUSB1044 Other Parts Discussed in Thread: TUSB1064 , , Hi expert,
My customer plan to design a USB-C I/O Hub like below Block diagram. There are 2 ports: I/O B connect to mother board(DFP), another port cnonnect to a UFP. Can you help to…
Part Number: TUSB1044 Hi Team,
Per our discussion in Email, please help check below questions:
USB3.0 10G and DP 5.4/8.1G power consumption
DP speed rate support
Do TUSB1044 support 8.1G/lane HBR3 to transmit 4K60 10bit, YUV444,YUV4:2:2,YUV4…
Part Number: TUSB1044A Other Parts Discussed in Thread: TPS65994AD , TUSB1044 , Hi sir,
I have some TUSB1044 EQ setting by TPS65994AD.
I got to know TPS65994AD write 6666, 8888, aaaa, cccc at 0x9 and 0xa address.
However, I don't know what 6666…
Part Number: TUSB1044 Other Parts Discussed in Thread: TUSB544 , Tool/software: Hi Team,
May I have your support to find a closet device here? Thanks!
USB Type-C Linear Redriver
Operating Voltage: 1.8V
USB Transmission: Supports USB 3.2 Gen1…
Part Number: TUSB1044 Hi Team,
Please help review the application circuit of TI device [TUSB1044RNQR] in our schematic. Attached is the PDF of this part of the schematic.
Please focus on checking if there are any issues or optimization suggestions…