Part Number: TUSB1044AEVM Other Parts Discussed in Thread: TUSB1044RNQEVM Subject: TUSB1044RNQEVM — request for PCB design files (Gerber / OrCAD / Allegro)
Hi TI team,
I'm working with the TUSB1044RNQEVM evaluation module and would like to request…
Part Number: TUSB1044RNQ
Hi TI Team,
I am working on a USB 3.2 Gen2 (10 Gbps) design and need clarification on selecting SRF value of AC-coupling capacitors for the differential data pair.
Self-Resonant Frequency (SRF): Many 100 nF MLCCs have SRF…
Part Number: TUSB1044RNQEVM Hi
This product has version A and B. Currently, we purchased version B, but the datasheet on your official website is version A
Please provide the following datasheet of version B
Thank you
Part Number: TUSB1044RNQEVM Tool/software: Hi
TUSB1044RNQEVMW uses a 5V power supply. If power is taken from the Type C plug and 100W is provided to the device connected to the Type C socket, does it require the addition of a PD controller with DRP…
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB1044 , TUSB1021Q1-EVM Tool/software: hi
we are working on the laptop project based on intel alder lake processor in which we are planning to use the two type c both supports USB+DP ALT…
Part Number: TUSB1044RNQEVM Tool/software: Hi, we are using TUSB 1044 for USB 3.2 gen 2 to DP (10gbps using all 4 lanes). Going through the specifications sheet, dont see any mention on its compatibility of P/N swap within a pair.
Can you please confirm…
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB1104 I tested TUSB1044RNQEVM because I want to design the USB redriver.
But I found the problem.
I don't want to use the USB 1:2MUX, then I want to set the USB 4 lane setting(RX1/TX1…
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB1044 We are using one part ( part no TUSB1044RNQR) in our design and we need the thermal data for this part for thermal simulation
Kindly provide the below thermal details for this parts…
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB216I Hi Sir,
My customer want to design a 10m active cable for type-c signal.
1. Is it ok to use TUSB1044EVM's circuit to meet customer's requirement? Where do we have to put the redriver…
Part Number: TUSB1044RNQEVM I got a TUSB1044RNQEVM from TI distributor. The board version is HSDC008B. How could I get the schematic file (.pdf is OK) for this version of EVM?
The schematic file available in the TI website is only for version HSDC008A…