Part Number: TUSB1046A-DCI Other Parts Discussed in Thread: SN65DSI86 Hi, TI expert.
The customer has an inquiry while reviewing the support of DP (Display Port) through USB-C on the board currently used. The composition of the board currently in use…
Part Number: TUSB1046A-DCI Other Parts Discussed in Thread: TPS65982 , TPS65987D , , TUSB1046-DCI , TUSB1064 Hello,
I designed a board that uses TUSB1046 to combine USB and DP to get USB-C. But I am unable to get it to work.
I came across the user guide…
Part Number: TUSB1046A-DCI Other Parts Discussed in Thread: HD3SS460 Hi Sir,
My customer is looking for an Alternate Mode device, they ask for the support of maximum cable length for TUSB1046A-DCI and HD3SS460?
Part Number: TUSB1046A-DCI Hi ,
We are using TUSB1046A-DCI one of our project for USB Host and DP port Source ALT MUX
Configurations:
USB DFP (Source side)
USB3.1 + 2Lane DP
GPIO Mode - I2C_EN( Pin 17 - Low)
CTL0 (Pin 22 - High (3.3V))
CTL1 (Pin 23 -…
Part Number: TUSB1046A-DCI Hi Expert,
customer only to use this device for programming, and won't to use display & AUX pin.
so how to connect displayport & AUX pin if no use them?
Regards,
Mark
Part Number: TUSB1046A-DCI Hi Team,
I understand from the E2E thread below that the unused DP 2-3 pins can be left floating. Our customer would like to confirm if the DP0, DP1 and AUX pins can be left floating or should be tied/pull down to ground.
https…
Part Number: TUSB1046A-DCI Other Parts Discussed in Thread: TUSB1046-DCI Hi,
If my customer want use TUSB1046A-DCI to replace TUSB1046-DCI, any thing need to be noticed?
Is it pin-to-pin replaceable? thanks!
Jeff
Part Number: TPS65987D Other Parts Discussed in Thread: TPS65987 , TPS25751 , TPS25730 , , TPS65994AE , TUSB1046A-DCI Tool/software: For TPS65987 USB PD Controller; Operating ambient temperature is –10°C - +125°C . But we need -30°C operating temperature…
Part Number: TUSB1046A-DCI Hello,
In my motherboard, I am using 4 x TUSB1046AI-DCI for 4 USB type C ports. 2 of the ICs are controlled by CYPD4226-40LQXIT . Our phase 1 design worked. We made some changes where we relocated the 4 x USBC to front panel and…