Part Number: TUSB1142 Other Parts Discussed in Thread: TPS25750 , TPS26750 Hi Team,
We operate the TUSB1142 via pin-strap. This means we can only select a linear mode – then the LFPS output signal is too low (750 mVpp). The LINR_L3 value for the LFPS…
Part Number: TUSB1142 Other Parts Discussed in Thread: STRIKE , Hi AE,
Regarding the RX path from the Type-C connector to the TUSB1142IRNQR, based on reference designs and project applications:
a. Is it acceptable to include AC coupling capacitors…
Part Number: TUSB1142 Hi AE,
The current Pre-Channel total and Post-Channel total are as follows.
Could you help recommend the appropriate settings for CEQ1, CEQ0 and SSEQ1, SSEQ0?
Type C Gen2
CEQ1
CEQ0
SSEQ1
SSEQ0
AEQENZ
AEQCFG…
Part Number: TUSB1142 Hi AE,
The current Pre-Channel total and Post-Channel total are as follows.
Could you help recommend the appropriate settings for CEQ1, CEQ0 and SSEQ1, SSEQ0?
Type C Gen2
CEQ1
CEQ0
SSEQ1
SSEQ0
AEQENZ
AEQCFG…
Part Number: TUSB1142 Hi Vishesh,
Thank you for your support!
Our disty FAE Bruce wants to discuss these issues with you, so we can talk detials here, thanks.
Hi Bruce,
I have sent Vishesh's reply to you, we can discuss here, but this is public…
Part Number: TUSB1142 Tool/software: Hi AE,
The datasheet of the TUSB1142 requires impedance control of 90 Ω ± 10% .
In the Intel PDG, the impedance control requirement is: Outer layer: 83 Ω ± 10%, Inner and outer layers: 85 Ω ± 10%.
What impedance…
Part Number: TUSB1142 Tool/software: Hi team
my customer are trying AEQ function with our TUSB1142 with competitor's, but they found ours AEQ result always read FF from 3B or 3C ,
they also try cable as short as 0.2M but still the same FF,
they…
Part Number: TUSB1142 Other Parts Discussed in Thread: TUSB1004 , , TUSB1104 Hi All,
Would you kindly tell us if IBIS-AMI models exist for TUSB1142I and TUSB1004?
Best regards, Shuhei Hayashi
Part Number: TUSB1142 Other Parts Discussed in Thread: TUSB321 , Tool/software: Hi,
I've implemented the attached circuit and works in USB-2 mode but not in USB-C mode.
USB-C should connect to a PC and USB-A will connect to one USB-3 camera.
If…
Part Number: TUSB1142 Hi AE,
The current Pre-Channel total and Post-Channel total are as follows. Could you help recommend the appropriate settings for CEQ1, CEQ0 and SSEQ1, SSEQ0?
project
CEQ1
CEQ0
SSEQ1
SSEQ0
…