Part Number: TUSB1146 Can the TUSB1146 be used for 10Gbps USB 3.2, to allow a Type-C cable on a downstream port to transfer data either flipped or not flipped?
Part Number: TUSB1146-Q1 Other Parts Discussed in Thread: TPS65987D , TUSB1146 Hello! I'm having a bit of trouble understanding what the "standard" firmware loaded into TUSB1146-Q1 and TPS65987D is and if it can support our application or not.
Our use…
Part Number: TUSB1146 Dear support team, refer to further case CS3204324 we're using the TUSB1146IRNQT for USB3.0 and Display Port but no power delivery.
But do we need a PD Controller as on your evaluation board TUSB1146EVM for the TUSB1146 and especially…
Part Number: TUSB1146 Other Parts Discussed in Thread: TPS65988 Tool/software: Hi Team,
We are using TUSB1146 & TPS65988 in our design. Could you kindly review the circuitry and provide you comments on this
Awaiting for your…
Part Number: TPS26750 Other Parts Discussed in Thread: TUSB217 , , TUSB1146 , TPS25751 , TPS25750 , TPD4S480 I have a USB 3.2 with Type-C connector for 10 Gbps data and power delivery. I'm using TPS26750, TPD4S480RUKR, TUSB1146 and TUSB217 together and…
Part Number: TPS25814 Other Parts Discussed in Thread: TUSB1146 , Hi sir,
Can TPS25814 match TUSB1146 for simply Type C non-PD USB3.2 Gen2 x1,10Gbps?
Non-PD, 5V/3A, source only
USB3.2 Gen2 x1,10Gbps, host only
If no, pls suggest a combo solution…
Part Number: TUSB1146 Tool/software: Hello:
Does TI have a suitable ALT MODE switching chip switch (supports switching two USB3.0 signals and four DP signals to one ALT MODE signal, and supports PD protocol chip)? You can refer to the following model…
Part Number: TUSB1146 Other Parts Discussed in Thread: TUSB1044 I'm working on a carrier for a COM-HPC Client SOM. I would like to add a USB-C port that supports USB 3.1 as well as display port alt mode.
I'm pretty new to USB-C, so apologies if I'm…