Part Number: TUSB1210-Q1 Tool/software: Hello,
I would like to know if this device comes in -55C to 125C operating temperature range?
best regards,
Michael kliem
Hi Zhou
①Thank you for your response. In abnormal situations, such as when an overvoltage is applied leading to overcurrent conditions, if a series resistor is used for current limiting, is overcurrent protection consideration necessary?
②What is…
Part Number: TUSB1210-Q1 Other Parts Discussed in Thread: TUSB8020B-Q1 Tool/software: Hi Expert,
Have a good day!
Does TI have USB HUB IC support carplay(Need Automotive rating)? I can't find it in ti.com and seismic.
Do we have plan to release…
Part Number: TUSB1210 HI,Team
I am considering whether to adopt TUSB1210 or TUSB1210-Q1. Please tell me the following about TUSB1210 and TUSB1210-Q1.
【question 1】 ・I checked the contents of the datasheets for the TUSB1210 and TUSB1210-Q1, but I couldn…
Part Number: TUSB1210-Q1 Tool/software: HI.all
Currently the project needs to find a transceiver similar to TUSB1210-Q1 with ULPI interface on the uplink and two USB2.0 interfaces on the downlink, does TI have a similar product? USB hubs and controllers…
Part Number: TUSB1210-Q1 Tool/software: May I connect 5V for VBAT voltage?
Figure 5 Host or OTG, ULPI Input Clock Mode Application Diagram
Figure 5 shows a diagram for connecting 3.1V-5.5V.
Part Number: TUSB1210-Q1 Tool/software: Hello, I have a question about estimating the maximum current consumption for components, both at typical and heightened temperatures
I am currently designing a circuit that is required to operate at extended…
Part Number: TUSB1210-Q1 Hi all,
I would like to know some questions about TUSB1210-Q1.
When using under the following conditions, the DP/DM is reversed.
This does not change even if register 0x08 is rewritten.
<conditions>
High-speed
Vbus…
Part Number: TUSB1210-Q1 Other Parts Discussed in Thread: TUSB1210 hi Team
Customer uses TUSB1210 to hang out of the FPGA with ULPI interface inside the FPGA to interface with TUSB1210, TUSB1210 to connect to the PC, would you like to ask if additional…
Part Number: TUSB1210-Q1 Team,
Could you confirm us, if the TUSB1210BRHBTQ1 and TUSB1210BRHBR are the same die?
What additional tests are performed for the Q1 qualification?
Thanks in advance.
- Needhu