Part Number: TUSB2046B Hello!
I've been working on an implementation of the TUSB2046B USB Hub. I believe I've set up the IC correctly, and can see it recognized by my Windows 11 laptop when it is plugged in (with and without the external EEPROM and…
Part Number: TUSB2046B Other Parts Discussed in Thread: TPS2044 I need someone to double-check our implementation of using the TUSB2046B hub to link several USB-C ports in USB 2 mode to a microcontroller.
We previously weren't able to get the three…
Part Number: TUSB2046B
Tool/software:
Hi,
We are facing the following issues for EFT/B test.
-EFT/B test
-Issues
1. The connection between the PC and the TUSB2046B is lost, and it does not recover automatically. (Low frequency)
2.…
Part Number: TUSB2046B Tool/software: I have previously gotten a TUSB2046B to work as a self-powered hub using reference designs, and peripheral devices successfully connected to a host. I am iterating on the design using a second TUSB2046B to connect…
Part Number: TUSB2046B Tool/software:
I am using the TUSB2046 as a hub for several on board devices.
The board is 2 layer
The bottom layer is poured as a ground plane
2 of the diff pairs are also on the bottom layer as highlighted in white on…
Part Number: TUSB2046B
Tool/software:
Hi TI,
We have connected the USB port of the MSP432 to a USB connector through the TUSB2046B hub. The TUSB2046B generates an event in which the result is an unknown device. If you baypass the TUSB2046B the USB…
Part Number: TUSB2046B Hello,
The M93C56 also has the auto-increment behavior required, but has more memory than the SGS-Thompson M936C46 that is named in the datasheet. I just wanted to confirm with you all that this will work still.
Thanks,
J…
Part Number: TUSB2046B Tool/software:
We are using the TUSB2046B USB hub IC in our project. While it works perfectly with standard USB peripherals such as flash memory, mouse, and keyboard, it fails to communicate with the WinCool S828G IC , which controls…
Part Number: TUSB2046B Other Parts Discussed in Thread: TMUXHS221 Hi Team,
Customer is using USB hub and 3 USB connectors on board, so is there any protection in HUB or any technique which can be implemented on board to prevents USB mass storage device…