Part Number: TUSB2077A Hi,
Good Day.
The customer is using the TUSB2077A and he sees that the recommender trace length is 8 inches, now how bad would it be to route the trace a little much longer, like around 10 or 11 inches without a bad interference…
Part Number: TUSB2077A Hi,
We are using TUSB2077 7-port hub circuit in one of industrial automation project.
The circuit is working ok. but our customer required below function.
1. In TUSB2077 how to avoid pen drive to detect at downstream USB ports…
Part Number: TUSB2077A Hi, TI Support Team
The customer is reviewing the application of TUSB2077A as a USB HUB IC.
Can it be applied as a USB TYPE-C product?
Please confirm.
Thanks.
Regards,
MJ
Part Number: TUSB2077A
Hello,
1) I was wondering about an APLL.
On page5 "datasheet", PIN Functions: MODE -> Mode select. When MODE is low, the APPL output clock is selected as the clock source ~~~
what is the full name of APLL?
2) Question…
Part Number: TUSB2077A Hi Team,
Some of the ports on TUSB2077A will not be used (ports 6 and 7) and therefore the overcurrent pins are not used. How should PWRON and OVRCUR for the respective ports be connected if they aren't used (pins 32,33,36,37…
Part Number: TUSB2077A At the moment, seems that I have done everything as per application and EVM, but I can’t have HUBCFG status to go HIGH. Also, it is not working: not seen as a device by the host.
It is a self-powered configuration (just like…
Part Number: TUSB2077A Hi team, My customer checked XRAY for TUSB2077A. The lead frame was different depending on the device. Is this a normal product? Please tell me why it is different. *This picture is the same lot. Sincerely. Kengo.
Part Number: TUSB2077A Hub not detect. Checked the Oscillator Pin its show 1.8Volt. Mode select as
PortPWR(41): 3.3V GANGED(8): 3.3V MODe(48): GND We tried by connecting the 1.5K Resistor between DP0 andsDP0PUR Even add the Oscillator series Resistor…