Part Number: TUSB215-Q1 Hello:
At present, My customer finds that Lotus has a demand for a front row Dual Port USB, which has two main functions:
(1) a USB port can support 60W fast charging; (2) Another port can support 27W fast charging and usb3…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB217 , TUSB215 , TUSB216-Q1 , TUSB216 , TUSB216I Hi experts,
TUSB217RGYRQ1 was design win on customer side. Due to the supply issue, they start to evaluate TUSB215-Q1. Can TUSB215…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , , TUSB217 , TUSB215 Hi, We used to use tusb217-q1, but for some reasons, we now replace it with tusb215-q1. However, the following problems occur when using tusb215-q1. Please analyze…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB213-Q1 Hi, For some reasons, we design the circuit of tusb215-q1 as shown in the figure below, that is, the 9th and 10th pins of tusb215-q1 are not connected, and the 5th and 6th…
Part Number: TUSB215-Q1 Hi all.
Hope you can help with an issue.
Designed a circuit following the design example. MID boost while using a thin 1m cable that runs near motors.
When the board was connected to PC (no slave device) it shows up as failed…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TPS2549 I have both TPS2549 and TUSB215-Q1 in our design and I am wondering how USB role switching can be handled?
Do I need to configure TUSB215-Q1 via I2C when our system is in device mode?…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TPS2549 , TUSB215 , TUSB214 Hi Sir
I saw TPS2549 have divider 3 and 1.2V detection
May I know TUSB215 can support apple 2.4A charge detection and samsung charge detection ?
Thanks
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB21 , TUSB211 , TUSB215 , TUSB215EVM Hi,
TUSB21 1 outputs the signal to detect USB device from DxM pins in the case of not connected USB device as follow thread.
Does the TUSB21 5 output…
Part Number: TUSB216 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB217A , TUSB213 , TUSB212 , TUSB215 , TUSB214 Tool/software: Hi team.
Could you please share the material to explain the difference between TUSB21x as below?
Part Number: TUSB215 Other Parts Discussed in Thread: TUSB212 Hello guys,
One of my customers is considering using TUSB215 for their new products.
At this moment, they have the following questions. Could you please give me your reply for them?
Q1…