Part Number: TUSB216I Hi Support Team,
I am reviewing the datasheet for the TUSB216I and noted the following statement: "The TUSB216I helps a system to pass the USB 2.0 high-speed near end eye compliance with a cable as long as 5 meters." Could you…
Part Number: TUSB216I Hi,
Based on the datasheet, the D1M pin need to connect to D2M and D1P pin need to connect to D2P, is it right? And we are afraid it is short circuit, thanks.
Part Number: TUSB216I Other Parts Discussed in Thread: TUSB216 , TUSB213 , TUSB212 Hi Team,
We are using the TUSB216IRWBR in our MB design and need the simulation model for channel analysis.
Could you please help us obtain the model as soon as possible…
Part Number: TUSB216I I want to increase Differential signal strength
I want to increase Dxp-DxM data signal amplitude to 2000 mV p-p is this device is capable of amplify signal to more then 800 mv.
800mV is the USB standard specification value
Part Number: TUSB216I Other Parts Discussed in Thread: TUSB212 , Hi,
Do we have the USB2.0 IBIS/S parameter model for SI simulation for TUSB216IRWBR? Thank you.
Best regards,
Randy
Part Number: TUSB216I Other Parts Discussed in Thread: TUSB216 Tool/software: Hi Team,
My customer has below application. I3C signal will go through TUSB216 redriver. Will this affect the I3C SI?
Thanks
Han
Part Number: TUSB216I Other Parts Discussed in Thread: TUSB216 Tool/software: Hey Team,
On the TUSB216I, if you have the boost set with a resistor on the BOOST pin, can that setting be overridden using I2C, or should the BOOST pin be left floating when…
Part Number: TUSB216I
Hi, Support Team
We consider TUSB216I to design 5 meter USB Cable, but some question as below
Q1: USB2.0 use 28AWG is workable?
Q2: as below chart: one side is FEMALE and aonther side is MALE, should we both side use TUSB216I…