Hi Hardy,
Are the USB2 pins on the USB-C receptacle shorted together? In the flip condition the eye is not boosted. I would recommend using TUSB216I for the best eye diagram.
Hi,
TUSB21x works with USB Type-C for USB 2 applications. TUSB212 has greater redriving capability over TUSB211. I would recommend using our latest TUSB216I which works as a signal conditioner and BC 1.2 controller. All devices can be used without any…
Hi Malik,
Yes, CD and ENA_HS are high during failure. The application of my customer should use the automotive qualified product, so TUSB216I can not use for that. I think that the setup(low or high) of DC_BOOST seems to be needed whether it works or…
Part Number: TUSB211 Other Parts Discussed in Thread: TUSB216I Hi
I need USB2.0 repeater for extenuation cable up to 10m from camera to cellphone
I bought the EVB SLLU246 that used with TUSB211 IC but this is not working properly.
Please let me know which…
HI,
The procedure you mentioned is what should be followed to have TUSB212 enter its test mode to boost test packets form the host. The goal here is to get TUSB212 CD pin low and ENA_HS pin high (this indicated test mode). In your procedure TUSB212 enters…
Hi Allan,
USB redriver placement recommendation is to place as close to the USB connector as possible. Without understanding the lose of the cables themselves between main board and I/O board it is hard to tell whether two TUSB212 would be needed. The…