Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217A-Q1 , TUSB216-Q1 , TUSB216 , TUSB217A , TUSB211A , TUSB211A-Q1 , TUSB216I Hi all,
Does the TUSB217-Q1 have an integrated CDP (charging downstream port)?
If so, what profile is this supplying…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB212-Q1 , TUSB217 , TUSB212 Hi Application Team:
We would like to use TUSB217-Q1 replace TUSB212-Q1 since USB2.0 SI on Type A port of C car is too weak to pass USB IF ,
we would like to know…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , , TUSB217 , TUSB215 Hi, We used to use tusb217-q1, but for some reasons, we now replace it with tusb215-q1. However, the following problems occur when using tusb215-q1. Please analyze…
Part Number: TUSB217-Q1 Hi,
Because the working voltage provided by our circuit to tusb217-q1 is not fixed, the range is 2.75V ~ 3.85v, and the voltage will change with the product working temperature (± 0.2V). Do the gain/sensitivity and other states…
Part Number: TUSB217-Q1 If a TUSB217-Q1 detects it has an I2C bus connected will the part still set the registers based on resistors connected to the RX_SEN and BOOST pins.
The datasheet seems to imply that the RX_SEN and BOOST pins would be ignored…
Part Number: TUSB215-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB217 , TUSB215 , TUSB216-Q1 , TUSB216 , TUSB216I Hi experts,
TUSB217RGYRQ1 was design win on customer side. Due to the supply issue, they start to evaluate TUSB215-Q1. Can TUSB215…
Part Number: TUSB213-Q1 Other Parts Discussed in Thread: TUSB217-Q1 , TUSB216-Q1 , TUSB217A-Q1
Our customer is looking for re-driver for their Automotive USB Charger application to meet CarPlay / Android Auto .
Is your recommend IC TUSB213-Q1 and…
Hi, For some reasons, we design the circuit of tusb217-q1 as shown in the figure below, that is, the 9th and 10th pins of tusb217-q1 are not connected, and the 5th and 6th pins are respectively connected to DP and DM signal lines. The reason why we do…
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217 Hi Sir,
Would you pls advise if TUSB217 either D1 or D2 can be HOST?
If yes, how to define which side is HOST? Thanks.
Thanks, Ian.
Part Number: TUSB217-Q1 Other Parts Discussed in Thread: TUSB217 Hi Sir,
We checked TUSB217 d/s found there are different comments for R setting.
Pls kindly check which one is correct, thanks.
RBOOST = 1.69K or1.8K?
R1 = 47K or 37K ?
R2 = 24K…