Part Number: TUSB320HAI Hi ,
When the system in suspend mode, I want to shutdown TSUSB320HAI to save power.
Does the ID pin has an known state in shutdown mode?
The similar question is below. Could you please open the answer?
https://e2e.ti.com…
Part Number: TUSB320HAI Other Parts Discussed in Thread: TUSB320LAI , TUSB319-Q1 Hi team,
May I know if we have pin to pin replacement with FUSB303BTMX and need AEC-Q100?
FUSB303BTMX d atasheet: https://www.onsemi.com/pdf/datasheet/fusb303b-d.pdf…
Part Number: TUSB320HAI Other Parts Discussed in Thread: TUSB320 Provide case details or comments: We expect the TUSB320 to become a sink when it is connected to an OTG device. We do have the rare case, that the USB320HAI forces source mode, when it should…
Part Number: TUSB320HAI Hi Team,
I would like to use TUSB320HAI as DFP.
I understand that TUSB320HAI supports USB Type-C™ Specification 1.1.
Can TUSB320HAI connect UFP device of USB Type-C™ Specification 1.3(Latest Rev)?
And, could you please…
Part Number: TUSB320HAI Hi Team,
We would like to use TUSB320HAI for UFP in GPIO mode.
Then, we have four questions.
-----------
[Q1]
We understand that “The VBUS_DET pin must be connected through a 900kohm resistor to VBUS on the Type-C…
Part Number: TUSB320HAI Other Parts Discussed in Thread: TUSB320 Hi Experts,
We received inquiries about DISABLE_RD_RP bit in CSR Registers( address = 0x45). Our customer is developing specific tow boards, as follows. The board1 has Type-C receptacle…
Part Number: TUSB320HAI Hi
We are using the TUSB320HAI in our USB C design as both a power source and power sink. (PORT pin left floating). We are using in h/w mode and have all other pins connected as per reference design.
From our testing the behavior…
Part Number: TUSB320HAI Other Parts Discussed in Thread: TUSB320LAI , TUSB320
Hi Team, My customer considers to use TUSB320HAI or TUSB320LAI for UFP application. 1) Is there any criteria to decide GPIO mode or I2C mode? I believe the difference is the…
Thanks for the solution.
But still it won't solve my Problem because of CAD limitation.
If you have such kind of Part which can meet CAD things then Please suggest rest we can close this query.
Thanks
Saumil
Part Number: TUSB320HAI Hi Team,
Our costumer are evaluating the dead battery mode using TUSB320HAIEVM.
However, TUSB320HAIEVM can’t receive VBUS voltage even if DFP device is connected.
We would like to know whether we can evaluate the dead battery…