Part Number: TUSB321 Hi TI team,
I am using the TUSB321RWBR as a CC controller. The circuit diagram is shown below. When I connect an external hub, I find that the DIR pin outputs a high level, which is not the expected low level. Then I removed the…
Part Number: TUSB321 Hi Experts,
The datasheet states to use 500k resistor for 1.5A. However, I cannot find one.
What is the minimum and the maximum value that I can use for this? will 510k work?
Regards,
Marvin
Part Number: TUSB321 Other Parts Discussed in Thread: AM62A3-Q1 , TUSB319-Q1 Tool/software: Hello Team ,
In our application we need to Negotiate for the with laptop for Current Advertisement (5V@3A) using the Standalone CC Controller in UFP(Sink) Configuration…
Part Number: TUSB321 Other Parts Discussed in Thread: TUSB320 In our host application we have USB-C DFP only port.
If no device is attached to the USB port the VBUS voltage must remain off.
Is it OK to turn on the VBUS voltage by the ID pin directly…
Part Number: TUSB321 Hello,
I know that the PORT pin samples its 3-level status at power up.
How much time after power up the device is still sampling the signal?
I want to add an option to present the value on PORT pin from external CPLD device…
Part Number: TUSB321 Tool/software: Hello,
My customer wants to use TUSB321 for a USB Type-C development project.
They are trying to process the CC line with TUSB321 in order to configure the product with all optical. Is normal operation possible…
Part Number: TUSB321AI Other Parts Discussed in Thread: TUSB321 , TUSB320 Tool/software: Hi
We want to use the TUSB321 in DRP (dual role port) mode. Therefore the PORT pin is unconnected. Do I need some resistors on my board on the CC pins or must they…
Part Number: TUSB321 Tool/software:
Hi TI Experts,
Please support the below query:
According to the TI's TUSB231 chip datasheet - the recommended external pull-up resistor attached to the TUSB321 USBC_ID output (open drain) shall be 200K.
In the…
Part Number: TUSB321 Tool/software: Hello,
I found some issue and I don't understand what is the problem with my circuit. Or maybe with your TUSB321 device.?
Datasheet specify in UFP mode (port = GND), the OUT1 and OUT2 pin signalize the Type-C current…