Part Number: TUSB321AI Other Parts Discussed in Thread: TUSB321 Hi Team,
We are using TUSB321A in one of our projects.
I'm using the TUSB321A as DFP configured according to the spec and the current mode is set to the Default current mode.
I'm…
Part Number: TUSB321 Hello~
There is two product using two TUSB321.
First product is DFP 0.9A setting and another is DFP 1.5A setting.
Case 1 is DFP 1.5A setting product in the second stage and DFP 0.9A setting product in the first stage.
…
Part Number: TUSB321 Other Parts Discussed in Thread: TUSB1104
Hello,
Currently, we are looking for USB 3.2 Gen 2x2, PHY, could please share the part number details & data sheet for the same.
Thanks, M. Reuel Joshua.
Part Number: TUSB321 Other Parts Discussed in Thread: TUSB320 Hi,
My customer needs to deliver <15W, the port will only power little dongles and won’t be sinking any power from the USB-C port.
The USB-C port will support a few functions:
Act as…
Part Number: TUSB321
Hey Expert,
I am looking for an USB component TUSB321, can you help clarify the application of this chip and USB nego mechanism when plugging a PD device with 9W consumption, thanks for support.
Jim
Part Number: TUSB321 Hello,
I'm trying to scope out a design where I will have a USB-C receptacle on one side and then route the nets to a USB-C plug. Essentially I'm trying to make a USB-C extender. Instead of routing all of the nets on the receptacle…
Part Number: TUSB321 Other Parts Discussed in Thread: , TUSB322I Hi team,
When TUSB321 is used to detect VBUS, how can we inform CPU if we detect VBUS? What feedback signals do we have?
Thank you very much for your help.
Best regards,
Part Number: TUSB321 Hi Support Team
We are using the USB CC controller TUSB321RWB with the USB MUX HD3SS3212RKS for meeting the functionality of the USB DFP port. Connected the load switch (limiting the current to 0.9A) to meet the requirement of…
Part Number: TUSB321 Hi,
As highlighted below, the USB Type-C specification states that "the Source can dynamically adjust the value of Rp to indicate a change in available USB Type-C Current to a Sink.".
I am wondering if this is something a TUSB321…
Part Number: TUSB321 Hi there,
I am designing a device with USB C receptacle connector. This port is used for USB 2.0 data communication, in addition to receiving power up to 5V 3A. When the device is connected to a laptop through a USB A port (on…