Part Number: TUSB321AI Hi,
The TUSB321AI datasheet (Revision A) states that "The PORT pin is only sampled at reset or power up."
Please define the reset condition(s).
Regards,
Kwun
Part Number: TUSB321AI We are a CynLr, a Robotics and Machine Vision startup.
We are working on including a USB 3.1 gen 1 5Gbps with Type-C for connecting a camera to PC. We need help in verifying the USB 3.1 portion with Type-C (Circuit in-between…
Part Number: TUSB321AI Hi All,
can you please tell if the TUSB321AI is in configure as UFP, and it will try to communicate out the power level that it can consume.
When it detects then he will tell the system through OUT1 and OUT2 the power that…
Part Number: TUSB321AI Hi Team,
My customer seems have the similar issue to the e2e thread " TUSB321 not detecting cable inversion " but TUSB321AI was used already.
They tried 3pcb and all of these DIR didn't change state at all when either CC1/CC2…
Part Number: TUSB321AI Other Parts Discussed in Thread: HD3SS3212 , TUSB321 Dear Brian,
can you please review the UBS UFP schematic that i sent you via e-mail?
Best Regards,
David.
Part Number: TUSB321AI Hi Experts, If Type-C-A conversion cable is connected to TUSB321AI (TUSB321AI is as DFP), how TUSB321AI will detect a type-c current? It will depend on CURRENT_MODE pin setting? Best Regards, Fujiwara
Part Number: TUSB321AI Hello Experts, I would like to know why RVBUS is specified in datasheet. The datasheet also stated RVBUS=900Kohm/1% resistor required, but there is no 900Kohm in standard value. So I would like to know the reason. If customer choose…
Part Number: TUSB321AI Other Parts Discussed in Thread: TUSB1044 , TUSB321 , TUSB1044RNQEVM
Hello TI experts,
My customer considers TUSB321AI while using TUSB1044.
actually I asked about TUSB1044, and another expert said that I have to use TUSB321…
Part Number: TUSB321AI Dear Sir:
In our system there are 2 power supply source, 1 is powered by USB, 2 is powered by POE.
In current system design, we use "CV_USB0_DETECT_VBUS” to detect USB insert or not.
If I powered by POE, the system could work…
Part Number: TUSB321AI Dear Sir:
In our system there are 2 power supply source, 1 is powered by USB, 2 is powered by POE.
In current system design, we use "CV_USB0_DETECT_VBUS ” to detect USB insert or not.
If I powered by POE, the system could…