Part Number: TUSB4020BI-Q1 Other Parts Discussed in Thread: TPS2561 Could you tell me the meaning of PWRCTL_POL in TUSB4020BI-Q1? I don't quite understand the function corresponding to the high and low status of this pin
Part Number: TUSB4020BI-Q1 A device attached to one of our TUSB4020BI-Q1 downstream ports needs to have it's power cycled occasionally.
Is it possible to do this via the TUSB4020BI-Q1 or would we need to add extra logic to the PWRCTL1 signal? (I couldn…
Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: TUSB4020BI-Q1 , Hi, Team
Hope you are doing well!
My customer is evaluating our TUSB8020B-Q1 and TUSB4020BI-Q1.
From their datasheets, they both need to use an external EEPROM.
When customer design…
Part Number: TUSB4020BI-Q1 Hi All,
We have 2 questions when using TUSB4020BI-Q1 .
1. Since we only need the TUSB4020BI-Q1 as a USB 2 HUB, no power switch or SMBus/I2C is needed.
May I know how to configure below pins?
SCL / SMBCLK (Pin 2) …
Part Number: TUSB4020BI-Q1 Other Parts Discussed in Thread: TUSB4020BI May I ask what is the voltage tolerance value of D+/- output of TUSB4020BI-Q1 HUB? It is not specified in the manual. Will D+ short circuit to VBUS 5V damage the HUB?
Part Number: TUSB4020BI-Q1 Hi,
I'd like to know why we can't see the USB 2.0 HUB in Linux using "lsusb" command.
we checked voltages:
1. VDD_1P1 (Equal to 1.16 on board)
2. VCC_3V3 (Equal to 3.34 on board)
Note: I understood the the EEPROM…
Part Number: TUSB4020BI-Q1 This is a new chip for me; the hub shows up on the host, both Windows and Linux, but windows indicated driver issues and Linux says "can't open device"... Anyone encounter this before?
Part Number: TUSB4020BI-Q1 Hello TI Forum,
I've made a LGA to USB adapter for IoT modules. For some reason the TUSB4020BI-Q1 draws alot of current from the 1.1 V LDO and it gets very hot. (And eventually breaks if supplied long enough).
I've so far…
Part Number: TUSB4020BI-Q1 Hello team,
I need to connect 2 USB devices to and HUB, one of them is High Speed (USB Audio Class 2.0) the other one is Full Speed (VCOM).
Can TUSB4020BI-Q1 support both of them at maximum allowed speed, especially USB audio…