Part Number: TUSB4041PAPEVM Hello!
Could you confirm that the EEPROM part recommended is the 24AA04-I/P? This is what is listed in the BOM, but on the schematic it is labeled as AT24C04.
Thanks,
Sarah
Part Number: TUSB4041PAPEVM It looks like J4 pin 7 is disconnected in the schematic and the layout. I assume it is a non-issue since it connects through the shield, but this is not consistent with the other connectors.
Part Number: TUSB4041PAPEVM Hi, do you know if two TUSB4041 connected with a 5m USB cable can comply 1kV Signalburst Test with Criteria B ?
(CritB: after the burst disturbance the connection should be reconnected without user action)
BR Martin
Part Number: TUSB4041PAPEVM TUSB4041 Support team
I would like to know the configuration data in OTP of TUSB4041 used in TUSB4041PAPEVM.
Regards,
Tamio
Part Number: TUSB4041PAPEVM Dear all
I would need the tool chain to incircuit program the EEPROM on the TUSB4041PAP, could you please also provide me
the correct drivers-kit for the device that opens up, when in EEPROM programming mode?
BR
Tes…