Hi Yongki:
If you have different I2C masters on single MCU like I2C#1, I2C#2...IC2#4, it should work., but you need to connect them separately.
I2C#1 to first TUSB422, .. I2C#4 to 4th TUSB422.
Best
Brian
Part Number: TUSB422 Tool/software: We built a tiny board with TUSB422 on it. We are supplying 3.3V to VDD and VCONN.
Our end-goal is to be able to read the emarker on the cable.
We have the cable plug into the board, and we tried to configure the chip…
Part Number: TUSB422 Other Parts Discussed in Thread: MSP430F5528 Tool/software: I am looking for a very low-cost small-footprint way to connect a phone, charger and an MSP430 device (MSP430F5528). The microcontroller has a small back up battery and the…
Grady:
From power consumer to power provider: (DRP):
5. Upon reception of PS_RDY message from port partner, change Role Control register to present a Rp.
6. Enable system source VBUS. TCPM should send SourceVbusDefaultVoltage command to TUSB422 Command…
Part Number: TUSB422 Other Parts Discussed in Thread: TCA9543A , TS5A23157 Dear Team,
Hope you are doing well!
Recently, our customer wants to use TUSB422 in new projects.
They want to know, how can TUSB422 support two different I2C addresses.
Could you…
Part Number: TUSB422 Hi team,
Support need!!!
When customers used tusb422 to connect to the C port of macbook, they found that TUSB422 could not receive the Get Source Cap Extended packet sent by mac. It timed out and did not reply, resulting in soft_reset…
Part Number: TUSB422
Hi team,
The customers use tusb422 to connect to the C port of the mac computer and cannot receive the Get Source Cap Extended packet sent by the mac. There is no reply after timeout, resulting in soft_reset. The mac would do it…
Hi TOnki:
Sorry for the late responce:
" WAIT " That is a SW feature. The TUSB422 doesn’t care since this is handled at a high level in software.
Regards
Brian