Part Number: TUSB422 Hi there,
the TUSB422 will send the vendor defined instruction when the adapter is plugged in/off frequently.
how can i remove the the vendor defined instruction?
BRs,
Shubiao
Part Number: TUSB422 Other Parts Discussed in Thread: TPS65987D The customer has a project which transform USBC port to DP port. (1 port USBC to 1 port DP dongle application)
I guess TUSB422+MSP430 could realize this function. Is it right?
Is there any…
Part Number: TUSB422 Hi,
I'm brainstorming how to implement a USB device that talks and provides power to a tablet via a type C connector (UFP + Power Source). I ran into this thread , which is precisely what I want. However, I'd like to reduce FW…
Part Number: TUSB422 Hi there,
In my application, I need to reset the TUSB422 sometimes; how can i modify the try_snk to Snk. is it feasible via software?
BRs,
Shubiao
Part Number: TUSB422 Hi there,
I need an annotation of PD 3.0 sample code of tusb422. as customer is developing the PPS function based on our PD3.0 sample code, we need a better understanding of the current sample code.
besides, the sample code doesn…
Part Number: TUSB422 Dear teams,
Based on the DS, it seems that TUSB422 can implement alternate mode with register 0x18 [3:2]. Could I ask normally how to identify one device to support alternate mode or not? Or we can say one device support alternate…
Part Number: TUSB422 Hi there,
I am very confused about the I2C data setup time of TUSB422.
it is said the min time of Tsu;dat is 50uS.
however, when the I2C clock frequency is 100khz, period is 10uS. that means 50uS is 5 period. that doesn't make sense…
Part Number: TUSB422 Other Parts Discussed in Thread: TUSB1146 , TPS25221 , TPS65987 Hi,
My customer using Type-C port to output 4 Lanes DP2.0 at alternative mode, and also need support PD output only 5V/900mA,
Could they use TUSB422 + TUSB1146 and one more…
Part Number: TUSB422 Dear teams,
Could I ask whether TUSB422 has portion of protocol layer to implement CRCReceiverTimer and RetryCounter since I can't find it in the DS? If it has, could you help share what is the advantages of implement CRCReceiverTimer…