Part Number: TUSB501 hi,
My customer is using TUSB501 on monitors for U3 type A port. USB IF will have FRI test. Can I know anything customer should be careful for this?
BR,
frank
Part Number: TUSB501 Other Parts Discussed in Thread: TUSB551 , TUSB1002A According to the USB3 specification , the U3 suspend current is limited to 2.5 mA. However, TUSB501 datasheet says that it consumes 6.1 mA in average in U2/U3 link state. As an additional…
Part Number: TUSB501-Q1 Other Parts Discussed in Thread: TUSB501 Hi
We know that redriver is to drive longer cable and PCB trace, however, is there any rule to determine how long cable(how many insertion loss) needs a USB3.0 redriver? Thanks.
Part Number: TUSB501-Q1 Other Parts Discussed in Thread: TUSB542 , TUSB1064 , TUSB564 , HD3SS3212-Q1
Hi, team,
We would like to place TUSB501-Q1 for USB3.0 with type-C port. Two questions may need your help on reply.
1. Is the re-driver only suggested…
Part Number: TUSB501
As shown in the above schematic, is it allowable to swap the plus and minus inputs on the IC. Understanding that I swapped them at both the input and output side of the chip. Is this okay to do to make PCB routing easier, or is…
Part Number: TUSB501 Other Parts Discussed in Thread: TUSB544 , TUSB1064 , TUSB564 , TUSB1044 Greetings,
Do you have an integrated product with PD,CC controller and USB 3.0 mux,
Any solution?
Thank u.
Part Number: TUSB501 Other Parts Discussed in Thread: TUSB211 Dear,
we saw TUSB211 (USB2.0) can support 5m cable, about(USB3.0) TUSB501 can support 5m cable?
If any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence.