Part Number: TUSB522P When the DE or EQ = floating, I measured 0.6 V on these pins with a multimeter.The datasheet states that the voltage on a floating pin should be 0.36·VCC; with VCC = 3.3 V this would be 1.188 V .Is the chip operating normally?
Part Number: TUSB522P Tool/software: Hello support team,
My customer is now evaluating the SI simulation for TUSB522P.
However, they cannot use our IBIS-AMI due to the compatibility.
Do we have PSPICE model for them to do the simulation?
Thanks…
Part Number: TUSB522P Tool/software: In the previous circuit version, the signal Eye High test failed (as shown in the attached image). Therefore, in this version, we have added the TUSB522P to re-drive the USB signal.
Do you have any recommended settings…
Part Number: TUSB522P Other Parts Discussed in Thread: TUSB211A , TUSB1002A , TUSB1004 Is there any plan to roadmap the USB3.2 Gen2 redriver with connection detect output pin?
For example, I'm looking for something that combines the functionality of…
Part Number: TUSB522P Hi expert,
Can you help to check whether TUSB552P can work with the insert loss of below application? Customer is using TUSB552P EVM in their system.
The system block diagram:
BRs,
Rannie
Part Number: TUSB522P Hi,
I purchased TUSB522P EVM. It works fine with USB port on a laptop. would like to test our USB3.0 cable with BERT Scope BSA286CL. I can't get the output through the EVM. Below is the block diagram I have for the test. the input…
Part Number: TUSB522P Tool/software:
I have J721e EVM with silicon version 1.0 , (image is attached), I want to connect the serial cameras (which I used with multides card of TDA2x evm), I want to know the suitable camera daughter card that fits to…
Part Number: TUSB522P Tool/software: Hi Brian,
As you mentioned in email, I post E2E here.
Below is the question list from customer:
The EQ/DE effect for long USB3.0 signal transmission (Application curve(eye-diagram) in near-end and far-end)…
Part Number: TUSB522P Tool/software: Hi AE,
We plans to use TUSB522P to replace PS8719 and PI3EQX7502BZDEX .
Please help share the colay guild reference documents for us.
Best Regards