Part Number: TPS65982 Hi,
In the TUSB546EVM, GPIO2 from TPS65982 is connect to the POL signal line. May I know how to enable the PD controller to output the logic according to the orientation of the cable plugged to the connector?
Thanks.
Part Number: TUSB546EVM Hi Team,
Our customer bought 2 TUSB546EVM evaluation modules which work fine with a resolution of 1280x720. But with a resolution of 1920x1080 they can't get a video output on the Type C USB of the two modules. Is there any settings…
Part Number: TUSB546EVM Other Parts Discussed in Thread: TUSB546A-DCI Hello Team,
I see in the INT017A-002 schematics that CAD_SNK pin is connected to 1.8V which in my view is not ok because this violates the data sheet:
Can you confirm this, please…
Part Number: TPS65982 Other Parts Discussed in Thread: TPS65987 Hi Team,
For our project, we got the TUSB546EVM board and used the TI Application Customization 6.1.3 to configured the TPS65982 onboard to initiate as DFP and supports Data role swap.…
Part Number: TUSB546EVM Other Parts Discussed in Thread: TUSB564 Hi USB-C team,
My customer is using TUSB564. They are planning on supporting DP alt mode (as UFP). They are also planning on supporting DRD too though.
They are new to USB-C and need…
Part Number: TUSB546EVM Hi team,
For this EVM schematic, I noticed the AUX_CH(p) and AUX_CH(n) lines have their pullups/pulldowns as NC. In addition, there are no AC coupling caps (instead there are 0 ohm resistors).
Why is this?
Thanks,
La…
Part Number: TUSB546EVM Other Parts Discussed in Thread: TPS65982 Dear all
I have one TUSB546EVM, and I take Apple adapter to power on, as below picture,but there is not 20V output on the J13 connector
My questions:
1. How to set the EVM,so…
Part Number: TUSB546EVM Hi,
I purchased a TUSB546EVM through Digikey in March this year. The EVM no longer works. It seems that U6 has failed as it becomes very hot as soon as USB type-B is connected. There is also visible damage on the top surface…
Hi~
I don't have TPS65982EVM board. Can I run the test in TUSB546EVM?
How can I control variable DC/DC controller circuit architecture?
Is there any way to handle it in H/W other than way to go in GUI?
Thanks.