Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: HD3SS3212 Tool/software: Hi everyone,
I designed a USB 3.0 hub using TI TUSB8020BPHP with Type-C upstream and downstream. Downstream Port 1 (to a CP2102 USB 2.0 device) works fine, but Downstream…
Part Number: TUSB8020B-Q1 Tool/software: I have completed and verified the schematic and PCB design using the TUSB8020BIPHPR USB hub controller. The IC is working correctly and the hub functionality is stable.
However, even under light load or idle…
Part Number: TUSB8020B Tool/software: Regarding the USB SS functionality, are there any signal integrity improvement of internal re-driving characteristics of this chip? Our board has a basics FR-4 dielectric, and a fairly long trace (7 inches). if we…
Part Number: TUSB8020B Tool/software: Hi Team,
There is a heating problem when the load is light. The HUB connects a USB3 (USB3 to EMMC) and a USB2 (LTE card) device
(1) When connected to USB3+USB2.0, 1V1 current consumption is 355mA 3V3 current consumption…
Part Number: TUSB8020B Tool/software: Dear TI Support Team,
I am currently working on a USB hub design using the TUSB8020B . I would like to kindly request a schematic review for the attached circuit.
In particular, I have a few questions:
I…
Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: TUSB8020B , TUSB8020BEVM Tool/software: Hello,
We are using USB Hub of TI, P/N: TUSB8020BIPHPQ1, interfaced to the USB Host controller of Xilinx Zynq Ultrascale+ MPSoC.
We are using petalinux…
Part Number: TUSB8020B Tool/software: Dear Sir or Madam
Could you please send me the software for programming the OTP memory
and the software for programming the external Eeprom? Are instructions included?
Thank you very much Yours sincerely M.…
Part Number: TUSB8020B I tried connect a 4TB external hard drive (Model:TS0GSJ25CK3, spec: 5V, 0.9A) to my TUSB8020B USB port but most of time it is unable to detect or sometime it will be cut off after a while.
Other thumb drives or external hard drive…
Part Number: TUSB8020B
Tool/software:
Hi Team,
ipmi power cycle
12V turn off, 5Vsb not turn off
hub ext port status failed
Is it caused by poor TX/RX signal quality? Or are there other reasons?