Part Number: TUSB8041-Q1 Tool/software: Dear TI Engineer,
We want to confirm that does TUSB8041-Q1 support entering power-saving mode without external device insertion, can you help confirm it? While when there is a external device inserted in and…
Part Number: TUSB8041 Hi Team,
I am using TUSB8041IPAPQ1 HUB for gateway project. I have one source USB 3.0 and USB 2.0 Ports. pls find the block diagram for the same below,
One output port of USB HUB USB 3.0 port connected to USB Type A connector…
Part Number: TUSB8041 Tool/software: Hi team,
if customer configure TUSB8041 as I2C master mode, but there isn't an EEPROM available, will TUSB8041 operate with default configuration? Thanks!
Rayna
Part Number: TUSB8041 Hello.
I checked the operation by configuring downstream 3.x A type circuit using the TUSB8041.
We connected a sensor with a C type interface to this board using an A-to-C cable.
After that, I added the cable circuit to the…
Part Number: TUSB8041 Other Parts Discussed in Thread: TUSB1142 Tool/software: Hi all, I am currently working on a board that utilizes the TUSB8041 hub along with the TUSB1142 USB-C MUX and the TPS25730D USB-PD controller. I am running into a strange…
Part Number: TUSB8041 Tool/software: Hello,
I have question regarding to TUSB8041 - 4 port USB 3.0 hub.
I will use two USB3.0 and two USB2.0 for downstream and i don't use it for battery charging application.
Can i floating(leave) below pins without…
Part Number: TUSB8041 Hi sir,
My customer use TUSB8041IRGCR and do 1000 times ON/OFF testing.
It happens to miss 5G module (Telit FN990A28) sometimes
AC power on/off test
AC on --> Turn on device and enter OS --> wait for 1m50s to detect USB…