Part Number: TUSB8042
Tool/software:
Hello~
I would like to control the tusb8042 PWR1~4 pins(Downstream ON/OFF Control) individually using vendor commands. Please provide me with relevant information on how to set the pins using vendor commands…
Part Number: TUSB8041 Hello,
I am using a TUSB8041 and would like to request the EEPROM programming tool and user guide.
Thank you for your support.
Kind regrads Valentin
Part Number: TUSB8042 Tool/software: This is Mihir Chauhan from Aimtron Technology Pvt.Ltd. We are working on an application project which is specifically used in audio domain. In this project, we have decided to use USB Hub which will be integrated with…
Part Number: TUSB8042 Tool/software: Hi,
I have tryout the TUSB8042 EEPROM Programming Utilities.
Question: After Flashing the EEPROM, it can no longer be Programmed again. Is there a OTP mechanism within the 8042 ?
Is there anyway to re-enter…
Part Number: TUSB8042 Tool/software: I want to individually control the PWR1-4 pins of the TUSB8042 with a C# program.
The purpose is to perform a hardware reset on a connected device at will while communicating with it using the libusb library.
Can…
Part Number: TUSB8042 Tool/software: Hi team,
I'm interfacing the TUSB8042 with a processor—do I need to swap the TX and RX lines for the SuperSpeed signals?
Currently, when I connect a USB 3.0 mass storage device to the port, it's only detected as…
Part Number: TUSB8042 Hi team,
This is for Samsung Monitor TUSB8042 we designed in 20Yr.
I believe TUSB8042 firmware should be updated via Microsoft Window.
But customer Samsung monitor asked “is there any firmware update for USB downstream…
Part Number: TUSB8042
Hello,
I am designing a board on which I use a TUSB8042 hub.
So, I would need the EEPROM utility for the TUSB8042.
How do I get it?
Best Regard.
Ryu
Part Number: TUSB8042 Hello,
we are using the TUSB8042 on our custom PCBs and are looking into a way to program the external EEPROM via USB.
I have seen a programming tool mentioned in the forums multiple times. Is it possible to get access to this…