Part Number: TUSB8044 Other Parts Discussed in Thread: , TUSB8042 , TUSB564 Tool/software: Dear support,
My customer is need to connect the USB 3.1 to 3 peripherals.
- 1 for USB 2.0,
- 1 for USB 3.1 Gen 1 charging/data transfer, and
- 1 for DP…
Part Number: TUSB8042 Hi, I would like to know about TI Tool and at what level of testing it can be used. We are currently considering testing a USBHUB with TUSB8042 implemented, and we think we can test the communication with TI Tool. Is it possible…
Part Number: TUSB8042 Hello Team,
in order to do a USB 3.0 pre-compliance tests: how to set the TUSB8042 into compliance mode to run the eye diagram test under Linux, please?
Thank you and Best Regards,
Hans
Part Number: TUSB8042 Other Parts Discussed in Thread: TUSB8043 , , TUSB8043A , TUSB8044 We plan to extend one of two USB ports on our SoM to two to four ports. We will embed the part on a Linux platform, but I don't see any SW interface beyond the on…
Part Number: TUSB8042 Other Parts Discussed in Thread: TUSB8041 , TUSB8044A Hi team,
May you provide the closest solution to replace RTS5411S-grt? Cross reference tool shows TUSB8041/2/3(A) are all functional similar? May you also briefly explain what…
Part Number: TUSB8042 I'm going to make a 1:4 hub using TUSB8042. I wrote the circuit by referring to the EVM circuit diagram, but I leave an inquiry to check the board before production.
I want to use EEPROM as the default setting.
SCHEMATIC1 _ 02…
Part Number: TUSB8042 Hello Team,
we are planning to use the TUSB8042 on a board but some pins will not be used.
Can you confirm the understanding below?
unused USB_SS_TX output pins can be left floating.
The datasheet says:
When the upstream…
Part Number: TUSB8042 Other Parts Discussed in Thread: TUSB8041 , Hi Team,
I am wondering how is the difference between TUSB8042 and TUSB8041. My client just asked about "USB Hub 1 to 4 is USB 3.1 gen1". Which one should I suggest to them? and how…
Part Number: TUSB8042 I have 4 ports on my board and want to control the power. I have the following connections on power-up:
p24 - GANGED pulled low p40 - FULLPWR... pulled low p41 - PWRCTL_POL Floating high p45 - AUTOENZ pulled low p39 - SMBUSZ -…
Part Number: TUSB8042 Hello JMMN and team
Currently my customer is under reviewing the power rail for TUSB8042.
And Is it sufficient of 1A for 1.1 and 3.3V rail?
Please review and let me get your advice on this.
Thanks and Best Regards
Billy…