Other Parts Discussed in Thread: TVP5146 HI I designed a board according evm6437,now i am puzzled by a problem,in my design, I just use one input channel of TVP5146,which is VI_1_A, but the design on evm board is VI_2_B for video in, so the example of…
Other Parts Discussed in Thread: TVP5146 My system is using synchronised video where I have data coming into a evmdm365 board via ethernet for every video frame (actually field so I have data on UDP coming in at 50Hz and video inside being processed at…
Other Parts Discussed in Thread: TVP5146 Hi,
We have begun routing the DM365 - TVP5146 traces. According to 'Application Note SLEA079' we have the following point:
Maintain good trace length matching of digital video output traces and clock.…
Other Parts Discussed in Thread: TVP5146 Dear experts,
In my application i am using CMOS sensor to capture image. I had already achieved it. My system was running fine. But due to some reason I had to reinstall my kernel on my board. I am using DM355…
Other Parts Discussed in Thread: TVP5146M2 , TVP5146 , TVP7002 Looking at the TVP5146M2 datasheet , it explicitly says that sync on green is not supported, and any references to RGB support refer to SCART, however I do not see this note in the TVP5146…
Other Parts Discussed in Thread: TVP5146 I have been working with the Davinci DM365 EVM board which has a TVP5146 part for composite video input. The board works great using the standard TVP5146 driver with color cameras, however it fails to auto detect…
Other Parts Discussed in Thread: TVP5146 Hi,
I use Video Input Daughtercard (DC-VIDEO-TVP5146N) with my FPGA Stratix II (DK-NIOS-2S60N) and with camera ACE-S360E (B&W, composite output). TVP5146 has next settings:
reg(0x00) = 0x05 reg(0x08) = 0x00…
Other Parts Discussed in Thread: TVP5146 I have a a LI-VI365 video capture board (composite and svideo) connected to a beagleboard-xm rev C. I want to run Linux on the beagle, and grab frames from the composite video input. The board has a TVP5146 chip…
Other Parts Discussed in Thread: TVP5146 I would like to detect when video source is connected to or disconnected from composite input on DM365EVM.
How can I setup TVP5146 video decoder and what registers need to be inspected afterwards in order to…