Part Number: TVS0701 Other Parts Discussed in Thread: AM26C31 , , TSD12C Tool/software: Hi team,
My customer is using AM26C31 and met the issue taht output port is short to GND.
Based on previous E2E link: https://e2e.ti.com/support/interface-group…
Part Number: TVS0701 Other Parts Discussed in Thread: ESD401 Tool/software: Dear Technical Support Team,
I'm looking for ESD protection for analog input/output.
Input/Output voltage is from 0V to 5V(DC level) and low leak current is required.
ESD…
Part Number: TVS0701 Other Parts Discussed in Thread: TVS3300 Hi E2E,
Good day.
For the TVS0701, the leakage current is ~0.25 to 40nA (at room temp) at 7V, the Vrwm. What is the expected leakage current below Vrwm? Is there an IV curve that shows…
Part Number: TVS0701 Hi,
Our customer is designing a medical sensor patch that needs AED defib protection at the electrode inputs according to IEC60601-2-27. They're used to using MAX30034 for clamping. Can TVS0701 replace MAX30034? I'm attaching a…
Part Number: TVS0701 Hi,
my customer needs 5V USB power line TVS, but the
IEC 61000-4-5 Current (8/20 µs), TA < 125°C
need to be at least 100A.
It seems that all our TVS current are less than 100A.
Do we plan to release higher current TVS?
Hello,
These devices have realized for sampling right now. For the full release schedule please email me at c-phillips@ti.com
Also yes they could put two of the unidirectional in anti series to make a bidirectional if that is preferred.
Part Number: AM26C31 Other Parts Discussed in Thread: TVS0701 , TSD12C Tool/software: Hi team,
My customer uses a lots of AM26C31IDR in Servo and VFD products.
Now they met a output waveform distortion issue of AM26C31 in servo products, which is…
Other Parts Discussed in Thread: TVS0701 , TPD1E10B06 Hi, TI Support Team
Please recommend a product that can be used as a substitute for the product below.
NSPM1041BMUTBG // ONSEMI
For reference, we plan to review the application to AI Speaker…
Part Number: TCAN334 Other Parts Discussed in Thread: TPD2E1B06 , TPD1E10B09 , TVS0701 , TPD4E101 , TCAN3413 , ESD2CAN24-Q1
Tool/software:
I am trying to diagnose why our CAN transceivers keep breaking somewhat arbitrarily when the modules are connected…
Part Number: SN65HVD3088E Other Parts Discussed in Thread: THVD1420 , THVD1520 , , TVS0701 , TPD1E10B09 Hi ,Experts
Here is a customer's RS485 project. when the customer use THVD1420, system can work normally at 10Mbps.
But if customer change THVD1420…